ERROR: v4l2 capture: mxc_v4l_dqueue() interrupt received

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ERROR: v4l2 capture: mxc_v4l_dqueue() interrupt received

2,920件の閲覧回数
kris_fei
Contributor III

Platform: IMX6DL
OS: Android 4.4

Kernel branch: 3.0.35

We ran Camera preview call back and 1080p video playback at the same time for about  6 hours.

Then error log as following:

<3>[111394.520272] ERROR: v4l2 capture: mxc_v4l_dqueue() interrupt received

<4>[111394.520832] VPU interrupt received.

<4>[111395.215555] imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00000001

<6>[111401.676261] binder: 2744:2744 transaction failed 29189, size 64-0

What's the reason? Is it related to memory?

ラベル(1)
5 返答(返信)

2,594件の閲覧回数
mkochy
Contributor I

any points as to where to look for such a bug?

 

660件の閲覧回数
segri544
Contributor II
I have the same problem. How did you solve the problem?
Thanks.
0 件の賞賛
返信

2,688件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Does the video stop after 6 hours?, or you are just receiveing the IPU warning after each N amount of frames?

0 件の賞賛
返信

2,688件の閲覧回数
kris_fei
Contributor III

The issue just happened after a long running time, maybe 6 hours or 8 hours.

And besides, camera can't capture data.

2,688件の閲覧回数
kris_fei
Contributor III

anyone replies?