EIM Synchronous mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EIM Synchronous mode

1,419 Views
thouswave
Contributor III

Hello, everyone

I have a project that use IMX6D EIM interface to communicate with FPGA, I have configured the EIM timing as:

    1. synchronous read/write mode

    2. MUM = 1, DSZ = 001, that is Multiplexed Address/Data mode and Data width is 16 bit。

When I read or write the EIM interface, The FPGA side sampling the bus signal with chip scope. We found that the address is increased by four, for example:

    0x00, 0x04, 0x08, 0x0C, 0x10, ......

That is confused, the data width is 16, address bus should increased by 2, why is 4?

anyone can help me?

Labels (3)
1 Reply

1,307 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Start access address depends on ARM instruction used for it.

Say, LDR is for 32-bit data and address is aligned for 32-bit.

LDRH : for 16-bit data.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply