RT patch for linux 3.0.35 on IM.X6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT patch for linux 3.0.35 on IM.X6

1,411件の閲覧回数
hongjunsong
Contributor I

Hi,

We are using IM.X6 with linux 3.0.35 from freescale for our real time application.  We found out the linux3.0.35 kernel cannot meet our real time requirements.  We are trying to apply the RT patch from https://rt.wiki.kernel.org/index.php/Main_Page​.  Once we applied the RT 3.0.35 patch for the freescale 3.0.35 linux, and found out that there are some files which cannot be patched.  We manually updated these files, and could build the kernel image.  However, the built kernel cannot run.

Later on, we found out the Freescale 3.0.35 is slight different from the official linux 3.0.35.  We would like to know anybody here could share any thought on this.

Regards,

Hongjun

ラベル(7)
0 件の賞賛
返信
1 返信

1,197件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi hongjun

for differencies one can look at

What the FSL Community BSP is not

FSL Community BSP Release Notes 1.8 documentation

also recommended to post this to meta-fsl-arm mailing list, so that more

people could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信