EIM Memory location and Multi Buffer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

EIM Memory location and Multi Buffer

跳至解决方案
1,238 次查看
villager
Contributor II

hello.
We are using imx6 and fpga connected by EIM bus.
When an interrupt occurs in the cpu, the data of CS0 is read from EIM Memory.
The structure is similar to the link below.
https://community.nxp.com/t5/i-MX-Processors/How-to-inteface-an-Xilinx-Artix-FPGA-to-the-imx6-dual-q...


We basically allocated CS0 as a 128M area.

I have a question.
1) Where is the physical location of this 128MB EIM memory?
Is it the internal memory of imx6 or the internal memory of fpga? Or is it external DDR memory?

2) We are using CS0 as a single buffer.
I want to use multi buffer like Ring buffer.
How do I start implementing it as a Ring buffer?
I would appreciate it if you could let me know the related application note or technical link.

Thank you so much, villager

0 项奖励
回复
1 解答
1,196 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For the EIM details, please read the EIM chapter 22 in the RM.

i.MX 6Dual/6Quad Applications Processor Reference Manual

 

And you could find some examples from google search about access external memory on EIM.

e.g.

https://community.toradex.com/t/accessing-external-memory-bus-eim-on-imx6-via-memory-map/6831

https://community.toradex.com/t/external-memory-bus-eim-on-imx6/6116

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,197 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For the EIM details, please read the EIM chapter 22 in the RM.

i.MX 6Dual/6Quad Applications Processor Reference Manual

 

And you could find some examples from google search about access external memory on EIM.

e.g.

https://community.toradex.com/t/accessing-external-memory-bus-eim-on-imx6-via-memory-map/6831

https://community.toradex.com/t/external-memory-bus-eim-on-imx6/6116

 

0 项奖励
回复