EIM Memory location and Multi Buffer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EIM Memory location and Multi Buffer

ソリューションへジャンプ
2,082件の閲覧回数
villager
Contributor II

hello.
We are using imx6 and fpga connected by EIM bus.
When an interrupt occurs in the cpu, the data of CS0 is read from EIM Memory.
The structure is similar to the link below.
https://community.nxp.com/t5/i-MX-Processors/How-to-inteface-an-Xilinx-Artix-FPGA-to-the-imx6-dual-q...


We basically allocated CS0 as a 128M area.

I have a question.
1) Where is the physical location of this 128MB EIM memory?
Is it the internal memory of imx6 or the internal memory of fpga? Or is it external DDR memory?

2) We are using CS0 as a single buffer.
I want to use multi buffer like Ring buffer.
How do I start implementing it as a Ring buffer?
I would appreciate it if you could let me know the related application note or technical link.

Thank you so much, villager

0 件の賞賛
返信
1 解決策
2,040件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

For the EIM details, please read the EIM chapter 22 in the RM.

i.MX 6Dual/6Quad Applications Processor Reference Manual

 

And you could find some examples from google search about access external memory on EIM.

e.g.

https://community.toradex.com/t/accessing-external-memory-bus-eim-on-imx6-via-memory-map/6831

https://community.toradex.com/t/external-memory-bus-eim-on-imx6/6116

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,041件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

For the EIM details, please read the EIM chapter 22 in the RM.

i.MX 6Dual/6Quad Applications Processor Reference Manual

 

And you could find some examples from google search about access external memory on EIM.

e.g.

https://community.toradex.com/t/accessing-external-memory-bus-eim-on-imx6-via-memory-map/6831

https://community.toradex.com/t/external-memory-bus-eim-on-imx6/6116

 

0 件の賞賛
返信