EGL problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EGL problems

2,022件の閲覧回数
RobSavoye
Contributor II

I'm trying to use the OpenVG support in L2.6.31_10.07.11_ER, and as far as I can tell, there is a bug in the lower level EGL support OpenVG depends on. ThIs is on a Freescale Babbage board. Basically eglInitialize() always returns a failure, yet the error code says success! If I force it to continue, it fails on the next EGL call, so it's definetely not initialized. The code I'm using runs on 3 other platforms, so I know it's not a code problem. Even eglinfo fails to initialize.

I'm now downloading the newer ltib sources from Freescale for L2.6.35_10.11.01_ER that I hope solves my problem. I figured it would be good to ask here, incase I'm just doing something stupid. I do have the amd_gpu_bin files installed, and the gpu driver is enabled in my kernel builds. I've also tried both the

gpu_z430 and gsl modules with no luck.

タグ(1)
0 件の賞賛
返信
1 返信

1,863件の閲覧回数
RobSavoye
Contributor II
Like usual, it takes posting a problem to fix it yourself! :-)
0 件の賞賛
返信