EGL problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EGL problems

1,981 Views
RobSavoye
Contributor II

I'm trying to use the OpenVG support in L2.6.31_10.07.11_ER, and as far as I can tell, there is a bug in the lower level EGL support OpenVG depends on. ThIs is on a Freescale Babbage board. Basically eglInitialize() always returns a failure, yet the error code says success! If I force it to continue, it fails on the next EGL call, so it's definetely not initialized. The code I'm using runs on 3 other platforms, so I know it's not a code problem. Even eglinfo fails to initialize.

I'm now downloading the newer ltib sources from Freescale for L2.6.35_10.11.01_ER that I hope solves my problem. I figured it would be good to ask here, incase I'm just doing something stupid. I do have the amd_gpu_bin files installed, and the gpu driver is enabled in my kernel builds. I've also tried both the

gpu_z430 and gsl modules with no luck.

Tags (1)
0 Kudos
Reply
1 Reply

1,822 Views
RobSavoye
Contributor II
Like usual, it takes posting a problem to fix it yourself! :-)
0 Kudos
Reply