ECSPI data tx/rx in LSB/MSB Control in iMX8MM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ECSPI data tx/rx in LSB/MSB Control in iMX8MM

跳至解决方案
1,248 次查看
sreedhar_appala
Contributor IV

Hi,

From the HW reference manual in iMX8MM of ECSPI

10.1.2.8 Byte Order
The ECSPI does not support byte re-ordering in hardware.

Is there any method / procedure to setup ECSPI for LSB or MSB first transfer

Thank you,

Sreedhar

0 项奖励
回复
1 解答
1,194 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

you are right, ECSPI hardware does not support byte re-ordering.

One will have to implement it in software.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,195 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

you are right, ECSPI hardware does not support byte re-ordering.

One will have to implement it in software.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复