How to place iMX8DXL into KS0 low power mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to place iMX8DXL into KS0 low power mode

600 Views
chirag_patel1
Contributor I

Does iMX8DXL automatically enter KS0 mode if only VDD_SNVS_4P2 pin is powered by 3.3V and 32kHz external crystal across RTC_XTALI/XTALO pins? If not, how do you enable KS0 low power mode?

What is the current draw in this mode when external 32kHz crystal is present versus external crystal not present?

0 Kudos
Reply
1 Reply

564 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chirags

you are right, power consumption details can be found in sect.4.1.1.

KS0 – SNVS-Only mode AN12338

i.MX 8QuadXPlus Power Consumption Measurement

sect.4.1.6 Low power mode supply currents

i.MX 8DualX Automotive and Infotainment Applications Processors

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply