Dual Screen with i.MX8M Plus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Dual Screen with i.MX8M Plus

跳至解决方案
3,559 次查看
Wobaffet
Senior Contributor I

Hello,

We will be using two screens. One will be LVDS 1280*800 and other one will be HDMI 1920*1080 with our i.MX8M Plus.

So can we run two different applications at both of our screens?

How would be the performance?

And I wonder if it is possible to make LVDS line 1-2 meters long?

Thank you in advance.

Best Regards.

Gencay Akyuz

0 项奖励
回复
1 解答
3,528 次查看
praveen_adi
NXP Employee
NXP Employee

Hi @Wobaffet , 

Using i.MX8MP, you can run two different applications on your screens.

The wayland/weston will occupy both the screens, enabling you to drag your applications/windows.

在原帖中查看解决方案

4 回复数
3,529 次查看
praveen_adi
NXP Employee
NXP Employee

Hi @Wobaffet , 

Using i.MX8MP, you can run two different applications on your screens.

The wayland/weston will occupy both the screens, enabling you to drag your applications/windows.

3,492 次查看
Wobaffet
Senior Contributor I
What do you think about the length of the LVDS line? How long can it be?
0 项奖励
回复
3,480 次查看
praveen_adi
NXP Employee
NXP Employee

It actually depends on your application / use case / screen size / cable type, etc.

The longer the cable, the higher would be the jitter inversely affecting the data rate. 

You may also want to refer to LVDS to HDMI adapter.

0 项奖励
回复
3,541 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Wobalfet,

 

Yes, it can ..

Regards

0 项奖励
回复