Dual Screen with i.MX8M Plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dual Screen with i.MX8M Plus

ソリューションへジャンプ
2,494件の閲覧回数
Wobaffet
Senior Contributor I

Hello,

We will be using two screens. One will be LVDS 1280*800 and other one will be HDMI 1920*1080 with our i.MX8M Plus.

So can we run two different applications at both of our screens?

How would be the performance?

And I wonder if it is possible to make LVDS line 1-2 meters long?

Thank you in advance.

Best Regards.

Gencay Akyuz

0 件の賞賛
返信
1 解決策
2,463件の閲覧回数
praveen_adi
NXP Employee
NXP Employee

Hi @Wobaffet , 

Using i.MX8MP, you can run two different applications on your screens.

The wayland/weston will occupy both the screens, enabling you to drag your applications/windows.

元の投稿で解決策を見る

4 返答(返信)
2,464件の閲覧回数
praveen_adi
NXP Employee
NXP Employee

Hi @Wobaffet , 

Using i.MX8MP, you can run two different applications on your screens.

The wayland/weston will occupy both the screens, enabling you to drag your applications/windows.

2,427件の閲覧回数
Wobaffet
Senior Contributor I
What do you think about the length of the LVDS line? How long can it be?
0 件の賞賛
返信
2,415件の閲覧回数
praveen_adi
NXP Employee
NXP Employee

It actually depends on your application / use case / screen size / cable type, etc.

The longer the cable, the higher would be the jitter inversely affecting the data rate. 

You may also want to refer to LVDS to HDMI adapter.

0 件の賞賛
返信
2,476件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Wobalfet,

 

Yes, it can ..

Regards

0 件の賞賛
返信