Dual FEC not working - extremely many RX errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dual FEC not working - extremely many RX errors

1,714件の閲覧回数
danielkleine-al
Contributor I

Dear community,

we try to get the two FECs on i.MX28 to run. Our hardware setup is that we have two Micrel KSZ8091 PHYs connected with a shared interrupt line. Software-wise we are running a Linux 4.4 kernel.

Our current status is that we

  • get a link on one or both ethernet interfaces as expected; speed auto-neg works; FEC interrupts work
  • link down / up (removing and plugging the cable) is working as expected
  • bootup looks good (both FECs and both PHYs detected and PHYs correctly assigned to the FECs)

The issue now is that whenever only a cable is plugged to eth0 we can send packets (and they look correct according to wireshark) but cannot receive anyhting.

As soon as we additionally connect a cable to eth1 we can send packets on both interfaces correctly and very randomly receive a valid packet; but most of the time only the RX frame error counter (as seen in ifconfig) goes up for eth0 and eth1.

Please let me know if anyone has also seen a similar behaviour or which further information I can provide? Thanks!

Excerpt from device tree:

mac0: ethernet@800f0000 {   phy-mode = "rmii";   phy-handle = <&phy0>;   pinctrl-names = "default";   pinctrl-0 = <&mac0_pins_a &mac0_rx_er>;   phy-supply = <&reg_dummy_3v3>;   phy-reset-gpios = <&gpio4 13 0>;   phy-reset-duration = <100>;   status = "okay";             mdio {     #address-cells = <1>;     #size-cells = <0>;     phy0: ethernet-phy@0 {                 interrupt-parent = <&gpio4>;                 interrupts = <5 8>;                 reg = <0>;     };        phy1: ethernet-phy@3 {                 interrupt-parent = <&gpio4>;                 interrupts = <5 8>;                 reg = <3>;        };        };
};
mac1: ethernet@800f4000 {   phy-mode = "rmii";   phy-handle = <&phy1>;   pinctrl-names = "default";   pinctrl-0 = <&mac1_pins_a &mac1_rx_er>;   phy-supply = <&reg_dummy_3v3>;   status = "okay";};
ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,569件の閲覧回数
danielkleine-al
Contributor I

Sorry - we have found the problem, ENET0_RXEN and ENET1_RXEN are interchanged on the layout.

0 件の賞賛
返信