Hi,
I am trying to bring up SD card in imx6Q sabreSD board using a hypervisor with virtio block feature. I would like to know the addresses and IRQ's I should use for this feature and what are the modifications in the dts file. Please share the DTS entry to be given for virtio block.
Regards, Prethibha
Is this feature supporting by a driver? or need any hardware support? (e.g. GPIO interrupt)
could you explain more about what is the requirement for the virtio block?
Thank you for responding jimmychan.
Yes, virtio block drivers are there in linux.(/drivers/block/virtio_block.c) and virtio interfaces in ./drivers/virtio
I'm exploring about the interrupts(which I'm unaware and need to know for SD card).
All I could find is for block device(SD card) to be available to the guest I need to make DTS entry and kernel configuration and also DTS entry in hypervisor.
The requirement for virtio block is
->I need SD card contents to be accessed from my guests(create/edit etc files) .
->The hypervisor I use doesn't have emulation for SD card and I cant'use passthrough(coz only one guest will be able to access SD card resources) but using virtio block it can be done.
And also as per the /drivers/block/virtio_mmio.c the DTS entry for any virtIO memory mapped device is as:
Device Tree node,
eg.:
virtio_block@1e000 {
compatible = "virtio,mmio";
reg = <0x1e000 0x100>;
interrupts = <42>;
}
Can I know how and from where the interrupts in DTS files are given?I refered the manual i.MX 6Dual/6Quad Applications Processor Reference Manual (REV 3).The addresses used are similar but interrupts are not.Is there any logic for the interrupts..?
I need the correct entries in DTS (I guess).I am not sure if there is any mapping of the interrupts to interrupt controller is also needed in the DTS.
I will attach the DTS file imx6qdl.dtsi.
/*
* Copyright 2011 Freescale Semiconductor, Inc.
* Copyright 2011 Linaro Ltd.
*
* The code contained herein is licensed under the GNU General Public
* License. You may obtain a copy of the GNU General Public License
* Version 2 or later at the following locations:
*
* http://www.opensource.org/licenses/gpl-license.html
* http://www.gnu.org/copyleft/gpl.html
*/
#include "skeleton.dtsi"
/ {
aliases {
/*gpio0 = &gpio1;
gpio1 = &gpio2;
gpio2 = &gpio3;
gpio3 = &gpio4;
gpio4 = &gpio5;
gpio5 = &gpio6;
gpio6 = &gpio7;*/
i2c0 = &i2c1;
i2c1 = &i2c2;
i2c2 = &i2c3;
serial0 = &uart1;
serial1 = &uart2;
serial2 = &uart3;
serial3 = &uart4;
serial4 = &uart5;
spi0 = &ecspi1;
spi1 = &ecspi2;
spi2 = &ecspi3;
spi3 = &ecspi4;
};
intc: interrupt-controller@00a01000 {
compatible = "arm,cortex-a9-gic";
#interrupt-cells = <3>;
#address-cells = <1>;
#size-cells = <1>;
interrupt-controller;
reg = <0x00a01000 0x1000>,
<0x00a00100 0x100>;
};
clocks {
#address-cells = <1>;
#size-cells = <0>;
ckil {
compatible = "fsl,imx-ckil", "fixed-clock";
clock-frequency = <32768>;
};
ckih1 {
compatible = "fsl,imx-ckih1", "fixed-clock";
clock-frequency = <0>;
};
osc {
compatible = "fsl,imx-osc", "fixed-clock";
clock-frequency = <24000000>;
};
};
soc {
#address-cells = <1>;
#size-cells = <1>;
compatible = "simple-bus";
interrupt-parent = <&intc>;
ranges;
dma_apbh: dma-apbh@00110000 {
compatible = "fsl,imx6q-dma-apbh", "fsl,imx28-dma-apbh";
reg = <0x00110000 0x2000>;
interrupts = <0 13 0x04>, <0 13 0x04>, <0 13 0x04>, <0 13 0x04>;
interrupt-names = "gpmi0", "gpmi1", "gpmi2", "gpmi3";
#dma-cells = <1>;
dma-channels = <4>;
clocks = <&clks 106>;
};
gpmi: gpmi-nand@00112000 {
compatible = "fsl,imx6q-gpmi-nand";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x00112000 0x2000>, <0x00114000 0x2000>;
reg-names = "gpmi-nand", "bch";
interrupts = <0 15 0x04>;
interrupt-names = "bch";
clocks = <&clks 152>, <&clks 153>, <&clks 151>,
<&clks 150>, <&clks 149>;
clock-names = "gpmi_io", "gpmi_apb", "gpmi_bch",
"gpmi_bch_apb", "per1_bch";
dmas = <&dma_apbh 0>;
dma-names = "rx-tx";
status = "disabled";
};
timer@00a00600 {
compatible = "arm,cortex-a9-twd-timer";
reg = <0x00a00600 0x20>;
interrupts = <1 13 0xf01>;
clocks = <&clks 15>;
};
L2: l2-cache@00a02000 {
compatible = "arm,pl310-cache";
reg = <0x00a02000 0x1000>;
interrupts = <0 92 0x04>;
cache-unified;
cache-level = <2>;
arm,tag-latency = <4 2 3>;
arm,data-latency = <4 2 3>;
};
pcie: pcie@0x01000000 {
compatible = "fsl,imx6q-pcie", "snps,dw-pcie";
reg = <0x01ffc000 0x4000>; /* DBI */
#address-cells = <3>;
#size-cells = <2>;
device_type = "pci";
ranges = <0x00000800 0 0x01f00000 0x01f00000 0 0x00080000 /* configuration space */
0x81000000 0 0 0x01f80000 0 0x00010000 /* downstream I/O */
0x82000000 0 0x01000000 0x01000000 0 0x00f00000>; /* non-prefetchable memory */
num-lanes = <1>;
interrupts = <0 123 0x04>;
clocks = <&clks 189>, <&clks 187>, <&clks 206>, <&clks 144>;
clock-names = "pcie_ref_125m", "sata_ref_100m", "lvds_gate", "pcie_axi";
status = "disabled";
};
pmu {
compatible = "arm,cortex-a9-pmu";
interrupts = <0 94 0x04>;
};
aips-bus@02000000 { /* AIPS1 */
compatible = "fsl,aips-bus", "simple-bus";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x02000000 0x100000>;
ranges;
spba-bus@02000000 {
compatible = "fsl,spba-bus", "simple-bus";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x02000000 0x40000>;
ranges;
spdif: spdif@02004000 {
compatible = "fsl,imx35-spdif";
reg = <0x02004000 0x4000>;
interrupts = <0 52 0x04>;
dmas = <&sdma 14 18 0>,
<&sdma 15 18 0>;
dma-names = "rx", "tx";
clocks = <&clks 197>, <&clks 3>,
<&clks 197>, <&clks 107>,
<&clks 0>, <&clks 118>,
<&clks 0>, <&clks 139>,
<&clks 0>;
clock-names = "core", "rxtx0",
"rxtx1", "rxtx2",
"rxtx3", "rxtx4",
"rxtx5", "rxtx6",
"rxtx7";
status = "disabled";
};
ecspi1: ecspi@02008000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6q-ecspi", "fsl,imx51-ecspi";
reg = <0x02008000 0x4000>;
interrupts = <0 31 0x04>;
clocks = <&clks 112>, <&clks 112>;
clock-names = "ipg", "per";
status = "disabled";
};
ecspi2: ecspi@0200c000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6q-ecspi", "fsl,imx51-ecspi";
reg = <0x0200c000 0x4000>;
interrupts = <0 32 0x04>;
clocks = <&clks 113>, <&clks 113>;
clock-names = "ipg", "per";
status = "disabled";
};
ecspi3: ecspi@02010000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6q-ecspi", "fsl,imx51-ecspi";
reg = <0x02010000 0x4000>;
interrupts = <0 33 0x04>;
clocks = <&clks 114>, <&clks 114>;
clock-names = "ipg", "per";
status = "disabled";
};
ecspi4: ecspi@02014000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6q-ecspi", "fsl,imx51-ecspi";
reg = <0x02014000 0x4000>;
interrupts = <0 34 0x04>;
clocks = <&clks 115>, <&clks 115>;
clock-names = "ipg", "per";
status = "disabled";
};
uart1: serial@02020000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x02020000 0x4000>;
interrupts = <0 26 0x04>;
clocks = <&clks 160>, <&clks 161>;
clock-names = "ipg", "per";
dmas = <&sdma 25 4 0>, <&sdma 26 4 0>;
dma-names = "rx", "tx";
status = "disabled";
};
esai: esai@02024000 {
reg = <0x02024000 0x4000>;
interrupts = <0 51 0x04>;
};
ssi1: ssi@02028000 {
compatible = "fsl,imx6q-ssi","fsl,imx21-ssi";
reg = <0x02028000 0x4000>;
interrupts = <0 46 0x04>;
clocks = <&clks 178>;
dmas = <&sdma 37 1 0>,
<&sdma 38 1 0>;
dma-names = "rx", "tx";
fsl,fifo-depth = <15>;
fsl,ssi-dma-events = <38 37>;
status = "disabled";
};
ssi2: ssi@0202c000 {
compatible = "fsl,imx6q-ssi","fsl,imx21-ssi";
reg = <0x0202c000 0x4000>;
interrupts = <0 47 0x04>;
clocks = <&clks 179>;
dmas = <&sdma 41 1 0>,
<&sdma 42 1 0>;
dma-names = "rx", "tx";
fsl,fifo-depth = <15>;
fsl,ssi-dma-events = <42 41>;
status = "disabled";
};
ssi3: ssi@02030000 {
compatible = "fsl,imx6q-ssi","fsl,imx21-ssi";
reg = <0x02030000 0x4000>;
interrupts = <0 48 0x04>;
clocks = <&clks 180>;
dmas = <&sdma 45 1 0>,
<&sdma 46 1 0>;
dma-names = "rx", "tx";
fsl,fifo-depth = <15>;
fsl,ssi-dma-events = <46 45>;
status = "disabled";
};
asrc: asrc@02034000 {
reg = <0x02034000 0x4000>;
interrupts = <0 50 0x04>;
};
spba@0203c000 {
reg = <0x0203c000 0x4000>;
};
};
vpu: vpu@02040000 {
reg = <0x02040000 0x3c000>;
interrupts = <0 3 0x04 0 12 0x04>;
};
aipstz@0207c000 { /* AIPSTZ1 */
reg = <0x0207c000 0x4000>;
};
pwm1: pwm@02080000 {
#pwm-cells = <2>;
compatible = "fsl,imx6q-pwm", "fsl,imx27-pwm";
reg = <0x02080000 0x4000>;
interrupts = <0 83 0x04>;
clocks = <&clks 62>, <&clks 145>;
clock-names = "ipg", "per";
};
pwm2: pwm@02084000 {
#pwm-cells = <2>;
compatible = "fsl,imx6q-pwm", "fsl,imx27-pwm";
reg = <0x02084000 0x4000>;
interrupts = <0 84 0x04>;
clocks = <&clks 62>, <&clks 146>;
clock-names = "ipg", "per";
};
pwm3: pwm@02088000 {
#pwm-cells = <2>;
compatible = "fsl,imx6q-pwm", "fsl,imx27-pwm";
reg = <0x02088000 0x4000>;
interrupts = <0 85 0x04>;
clocks = <&clks 62>, <&clks 147>;
clock-names = "ipg", "per";
};
pwm4: pwm@0208c000 {
#pwm-cells = <2>;
compatible = "fsl,imx6q-pwm", "fsl,imx27-pwm";
reg = <0x0208c000 0x4000>;
interrupts = <0 86 0x04>;
clocks = <&clks 62>, <&clks 148>;
clock-names = "ipg", "per";
};
can1: flexcan@02090000 {
compatible = "fsl,imx6q-flexcan";
reg = <0x02090000 0x4000>;
interrupts = <0 110 0x04>;
clocks = <&clks 108>, <&clks 109>;
clock-names = "ipg", "per";
};
can2: flexcan@02094000 {
compatible = "fsl,imx6q-flexcan";
reg = <0x02094000 0x4000>;
interrupts = <0 111 0x04>;
clocks = <&clks 110>, <&clks 111>;
clock-names = "ipg", "per";
};
gpt: gpt@02098000 {
compatible = "fsl,imx6q-gpt", "fsl,imx31-gpt";
reg = <0x02098000 0x4000>;
interrupts = <0 55 0x04>;
clocks = <&clks 119>, <&clks 120>;
clock-names = "ipg", "per";
};
/*gpio1: gpio@0209c000 {
compatible = "fsl,imx6q-gpio", "fsl,imx35-gpio";
reg = <0x0209c000 0x4000>;
interrupts = <0 66 0x04 0 67 0x04>;
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio2: gpio@020a0000 {
compatible = "fsl,imx6q-gpio", "fsl,imx35-gpio";
reg = <0x020a0000 0x4000>;
interrupts = <0 68 0x04 0 69 0x04>;
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio3: gpio@020a4000 {
compatible = "fsl,imx6q-gpio", "fsl,imx35-gpio";
reg = <0x020a4000 0x4000>;
interrupts = <0 70 0x04 0 71 0x04>;
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio4: gpio@020a8000 {
compatible = "fsl,imx6q-gpio", "fsl,imx35-gpio";
reg = <0x020a8000 0x4000>;
interrupts = <0 72 0x04 0 73 0x04>;
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio5: gpio@020ac000 {
compatible = "fsl,imx6q-gpio", "fsl,imx35-gpio";
reg = <0x020ac000 0x4000>;
interrupts = <0 74 0x04 0 75 0x04>;
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
};
gpio6: gpio@020b0000 {
compatible = "fsl,imx6q-gpio", "fsl,imx35-gpio";
reg = <0x020b0000 0x4000>;
interrupts = <0 76 0x04 0 77 0x04>;
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
};*/
gpio7: gpio@020b4000 {
compatible = "fsl,imx6q-gpio", "fsl,imx35-gpio";
reg = <0x020b4000 0x4000>;
interrupts = <0 78 0x04 0 79 0x04>;
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
};
kpp: kpp@020b8000 {
reg = <0x020b8000 0x4000>;
interrupts = <0 82 0x04>;
};
wdog1: wdog@020bc000 {
compatible = "fsl,imx6q-wdt", "fsl,imx21-wdt";
reg = <0x020bc000 0x4000>;
interrupts = <0 80 0x04>;
clocks = <&clks 0>;
};
wdog2: wdog@020c0000 {
compatible = "fsl,imx6q-wdt", "fsl,imx21-wdt";
reg = <0x020c0000 0x4000>;
interrupts = <0 81 0x04>;
clocks = <&clks 0>;
status = "disabled";
};
clks: ccm@020c4000 {
compatible = "fsl,imx6q-ccm";
reg = <0x020c4000 0x4000>;
interrupts = <0 87 0x04 0 88 0x04>;
#clock-cells = <1>;
};
anatop: anatop@020c8000 {
compatible = "fsl,imx6q-anatop", "syscon", "simple-bus";
reg = <0x020c8000 0x1000>;
interrupts = <0 49 0x04 0 54 0x04 0 127 0x04>;
regulator-1p1@110 {
compatible = "fsl,anatop-regulator";
regulator-name = "vdd1p1";
regulator-min-microvolt = <800000>;
regulator-max-microvolt = <1375000>;
regulator-always-on;
anatop-reg-offset = <0x110>;
anatop-vol-bit-shift = <8>;
anatop-vol-bit-width = <5>;
anatop-min-bit-val = <4>;
anatop-min-voltage = <800000>;
anatop-max-voltage = <1375000>;
};
regulator-3p0@120 {
compatible = "fsl,anatop-regulator";
regulator-name = "vdd3p0";
regulator-min-microvolt = <2800000>;
regulator-max-microvolt = <3150000>;
regulator-always-on;
anatop-reg-offset = <0x120>;
anatop-vol-bit-shift = <8>;
anatop-vol-bit-width = <5>;
anatop-min-bit-val = <0>;
anatop-min-voltage = <2625000>;
anatop-max-voltage = <3400000>;
};
regulator-2p5@130 {
compatible = "fsl,anatop-regulator";
regulator-name = "vdd2p5";
regulator-min-microvolt = <2000000>;
regulator-max-microvolt = <2750000>;
regulator-always-on;
anatop-reg-offset = <0x130>;
anatop-vol-bit-shift = <8>;
anatop-vol-bit-width = <5>;
anatop-min-bit-val = <0>;
anatop-min-voltage = <2000000>;
anatop-max-voltage = <2750000>;
};
reg_arm: regulator-vddcore@140 {
compatible = "fsl,anatop-regulator";
regulator-name = "cpu";
regulator-min-microvolt = <725000>;
regulator-max-microvolt = <1450000>;
regulator-always-on;
anatop-reg-offset = <0x140>;
anatop-vol-bit-shift = <0>;
anatop-vol-bit-width = <5>;
anatop-delay-reg-offset = <0x170>;
anatop-delay-bit-shift = <24>;
anatop-delay-bit-width = <2>;
anatop-min-bit-val = <1>;
anatop-min-voltage = <725000>;
anatop-max-voltage = <1450000>;
};
reg_pu: regulator-vddpu@140 {
compatible = "fsl,anatop-regulator";
regulator-name = "vddpu";
regulator-min-microvolt = <725000>;
regulator-max-microvolt = <1450000>;
regulator-always-on;
anatop-reg-offset = <0x140>;
anatop-vol-bit-shift = <9>;
anatop-vol-bit-width = <5>;
anatop-delay-reg-offset = <0x170>;
anatop-delay-bit-shift = <26>;
anatop-delay-bit-width = <2>;
anatop-min-bit-val = <1>;
anatop-min-voltage = <725000>;
anatop-max-voltage = <1450000>;
};
reg_soc: regulator-vddsoc@140 {
compatible = "fsl,anatop-regulator";
regulator-name = "vddsoc";
regulator-min-microvolt = <725000>;
regulator-max-microvolt = <1450000>;
regulator-always-on;
anatop-reg-offset = <0x140>;
anatop-vol-bit-shift = <18>;
anatop-vol-bit-width = <5>;
anatop-delay-reg-offset = <0x170>;
anatop-delay-bit-shift = <28>;
anatop-delay-bit-width = <2>;
anatop-min-bit-val = <1>;
anatop-min-voltage = <725000>;
anatop-max-voltage = <1450000>;
};
};
/*tempmon: tempmon {
compatible = "fsl,imx6q-tempmon";
interrupts = <0 49 0x04>;
fsl,tempmon = <&anatop>;
fsl,tempmon-data = <&ocotp>;
};*/
usbphy1: usbphy@020c9000 {
compatible = "fsl,imx6q-usbphy", "fsl,imx23-usbphy";
reg = <0x020c9000 0x1000>;
interrupts = <0 44 0x04>;
clocks = <&clks 182>;
};
usbphy2: usbphy@020ca000 {
compatible = "fsl,imx6q-usbphy", "fsl,imx23-usbphy";
reg = <0x020ca000 0x1000>;
interrupts = <0 45 0x04>;
clocks = <&clks 183>;
};
/*snvs@020cc000 {
compatible = "fsl,sec-v4.0-mon", "simple-bus";
#address-cells = <1>;
#size-cells = <1>;
ranges = <0 0x020cc000 0x4000>;
snvs-rtc-lp@34 {
compatible = "fsl,sec-v4.0-mon-rtc-lp";
reg = <0x34 0x58>;
interrupts = <0 19 0x04 0 20 0x04>;
};
};*/
epit1: epit@020d0000 { /* EPIT1 */
reg = <0x020d0000 0x4000>;
interrupts = <0 56 0x04>;
};
epit2: epit@020d4000 { /* EPIT2 */
reg = <0x020d4000 0x4000>;
interrupts = <0 57 0x04>;
};
src: src@020d8000 {
compatible = "fsl,imx6q-src", "fsl,imx51-src";
reg = <0x020d8000 0x4000>;
interrupts = <0 91 0x04 0 96 0x04>;
#reset-cells = <1>;
};
/* gpc: gpc@020dc000 {
compatible = "fsl,imx6q-gpc";
reg = <0x020dc000 0x4000>;
interrupts = <0 89 0x04 0 90 0x04>;
};
*/
gpc: gpc@020dc000 {
compatible = "fsl,imx6q-gpc";
reg = <0x020dc000 0x4000>;
interrupt-controller;
#interrupt-cells = <3>;
interrupts = <0 91 0x04 0 96 0x04>;
interrupt-parent = <&intc>;
pu-supply = <®_pu>;
#power-domain-cells = <1>;
};
gpr: iomuxc-gpr@020e0000 {
compatible = "fsl,imx6q-iomuxc-gpr", "syscon";
reg = <0x020e0000 0x38>;
};
iomuxc: iomuxc@020e0000 {
compatible = "fsl,imx6dl-iomuxc", "fsl,imx6q-iomuxc";
reg = <0x020e0000 0x4000>;
audmux {
pinctrl_audmux_1: audmux-1 {
fsl,pins = <
MX6QDL_PAD_SD2_DAT0__AUD4_RXD 0x80000000
MX6QDL_PAD_SD2_DAT3__AUD4_TXC 0x80000000
MX6QDL_PAD_SD2_DAT2__AUD4_TXD 0x80000000
MX6QDL_PAD_SD2_DAT1__AUD4_TXFS 0x80000000
>;
};
pinctrl_audmux_2: audmux-2 {
fsl,pins = <
MX6QDL_PAD_CSI0_DAT7__AUD3_RXD 0x80000000
MX6QDL_PAD_CSI0_DAT4__AUD3_TXC 0x80000000
MX6QDL_PAD_CSI0_DAT5__AUD3_TXD 0x80000000
MX6QDL_PAD_CSI0_DAT6__AUD3_TXFS 0x80000000
>;
};
pinctrl_audmux_3: audmux-3 {
fsl,pins = <
MX6QDL_PAD_DISP0_DAT16__AUD5_TXC 0x80000000
MX6QDL_PAD_DISP0_DAT18__AUD5_TXFS 0x80000000
MX6QDL_PAD_DISP0_DAT19__AUD5_RXD 0x80000000
>;
};
};
ecspi1 {
pinctrl_ecspi1_1: ecspi1grp-1 {
fsl,pins = <
MX6QDL_PAD_EIM_D17__ECSPI1_MISO 0x100b1
MX6QDL_PAD_EIM_D18__ECSPI1_MOSI 0x100b1
MX6QDL_PAD_EIM_D16__ECSPI1_SCLK 0x100b1
>;
};
pinctrl_ecspi1_2: ecspi1grp-2 {
fsl,pins = <
MX6QDL_PAD_KEY_COL1__ECSPI1_MISO 0x100b1
MX6QDL_PAD_KEY_ROW0__ECSPI1_MOSI 0x100b1
MX6QDL_PAD_KEY_COL0__ECSPI1_SCLK 0x100b1
>;
};
};
ecspi3 {
pinctrl_ecspi3_1: ecspi3grp-1 {
fsl,pins = <
MX6QDL_PAD_DISP0_DAT2__ECSPI3_MISO 0x100b1
MX6QDL_PAD_DISP0_DAT1__ECSPI3_MOSI 0x100b1
MX6QDL_PAD_DISP0_DAT0__ECSPI3_SCLK 0x100b1
>;
};
};
enet {
pinctrl_enet_1: enetgrp-1 {
fsl,pins = <
MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x1b0b0
MX6QDL_PAD_ENET_MDC__ENET_MDC 0x1b0b0
MX6QDL_PAD_RGMII_TXC__RGMII_TXC 0x1b0b0
MX6QDL_PAD_RGMII_TD0__RGMII_TD0 0x1b0b0
MX6QDL_PAD_RGMII_TD1__RGMII_TD1 0x1b0b0
MX6QDL_PAD_RGMII_TD2__RGMII_TD2 0x1b0b0
MX6QDL_PAD_RGMII_TD3__RGMII_TD3 0x1b0b0
MX6QDL_PAD_RGMII_TX_CTL__RGMII_TX_CTL 0x1b0b0
MX6QDL_PAD_ENET_REF_CLK__ENET_TX_CLK 0x1b0b0
MX6QDL_PAD_RGMII_RXC__RGMII_RXC 0x1b0b0
MX6QDL_PAD_RGMII_RD0__RGMII_RD0 0x1b0b0
MX6QDL_PAD_RGMII_RD1__RGMII_RD1 0x1b0b0
MX6QDL_PAD_RGMII_RD2__RGMII_RD2 0x1b0b0
MX6QDL_PAD_RGMII_RD3__RGMII_RD3 0x1b0b0
MX6QDL_PAD_RGMII_RX_CTL__RGMII_RX_CTL 0x1b0b0
MX6QDL_PAD_GPIO_16__ENET_REF_CLK 0x4001b0a8
>;
};
pinctrl_enet_2: enetgrp-2 {
fsl,pins = <
MX6QDL_PAD_KEY_COL1__ENET_MDIO 0x1b0b0
MX6QDL_PAD_KEY_COL2__ENET_MDC 0x1b0b0
MX6QDL_PAD_RGMII_TXC__RGMII_TXC 0x1b0b0
MX6QDL_PAD_RGMII_TD0__RGMII_TD0 0x1b0b0
MX6QDL_PAD_RGMII_TD1__RGMII_TD1 0x1b0b0
MX6QDL_PAD_RGMII_TD2__RGMII_TD2 0x1b0b0
MX6QDL_PAD_RGMII_TD3__RGMII_TD3 0x1b0b0
MX6QDL_PAD_RGMII_TX_CTL__RGMII_TX_CTL 0x1b0b0
MX6QDL_PAD_ENET_REF_CLK__ENET_TX_CLK 0x1b0b0
MX6QDL_PAD_RGMII_RXC__RGMII_RXC 0x1b0b0
MX6QDL_PAD_RGMII_RD0__RGMII_RD0 0x1b0b0
MX6QDL_PAD_RGMII_RD1__RGMII_RD1 0x1b0b0
MX6QDL_PAD_RGMII_RD2__RGMII_RD2 0x1b0b0
MX6QDL_PAD_RGMII_RD3__RGMII_RD3 0x1b0b0
MX6QDL_PAD_RGMII_RX_CTL__RGMII_RX_CTL 0x1b0b0
>;
};
pinctrl_enet_3: enetgrp-3 {
fsl,pins = <
MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x1b0b0
MX6QDL_PAD_ENET_MDC__ENET_MDC 0x1b0b0
MX6QDL_PAD_RGMII_TXC__RGMII_TXC 0x1b0b0
MX6QDL_PAD_RGMII_TD0__RGMII_TD0 0x1b0b0
MX6QDL_PAD_RGMII_TD1__RGMII_TD1 0x1b0b0
MX6QDL_PAD_RGMII_TD2__RGMII_TD2 0x1b0b0
MX6QDL_PAD_RGMII_TD3__RGMII_TD3 0x1b0b0
MX6QDL_PAD_RGMII_TX_CTL__RGMII_TX_CTL 0x1b0b0
MX6QDL_PAD_ENET_REF_CLK__ENET_TX_CLK 0x1b0b0
MX6QDL_PAD_RGMII_RXC__RGMII_RXC 0x1b0b0
MX6QDL_PAD_RGMII_RD0__RGMII_RD0 0x1b0b0
MX6QDL_PAD_RGMII_RD1__RGMII_RD1 0x1b0b0
MX6QDL_PAD_RGMII_RD2__RGMII_RD2 0x1b0b0
MX6QDL_PAD_RGMII_RD3__RGMII_RD3 0x1b0b0
MX6QDL_PAD_RGMII_RX_CTL__RGMII_RX_CTL 0x1b0b0
MX6QDL_PAD_ENET_TX_EN__ENET_TX_EN 0x1b0b0
>;
};
};
esai {
pinctrl_esai_1: esaigrp-1 {
fsl,pins = <
MX6QDL_PAD_ENET_RXD0__ESAI_TX_HF_CLK 0x1b030
MX6QDL_PAD_ENET_CRS_DV__ESAI_TX_CLK 0x1b030
MX6QDL_PAD_ENET_RXD1__ESAI_TX_FS 0x1b030
MX6QDL_PAD_ENET_TX_EN__ESAI_TX3_RX2 0x1b030
MX6QDL_PAD_ENET_TXD1__ESAI_TX2_RX3 0x1b030
MX6QDL_PAD_ENET_TXD0__ESAI_TX4_RX1 0x1b030
MX6QDL_PAD_ENET_MDC__ESAI_TX5_RX0 0x1b030
MX6QDL_PAD_NANDF_CS2__ESAI_TX0 0x1b030
MX6QDL_PAD_NANDF_CS3__ESAI_TX1 0x1b030
>;
};
pinctrl_esai_2: esaigrp-2 {
fsl,pins = <
MX6QDL_PAD_ENET_CRS_DV__ESAI_TX_CLK 0x1b030
MX6QDL_PAD_ENET_RXD1__ESAI_TX_FS 0x1b030
MX6QDL_PAD_ENET_TX_EN__ESAI_TX3_RX2 0x1b030
MX6QDL_PAD_GPIO_5__ESAI_TX2_RX3 0x1b030
MX6QDL_PAD_ENET_TXD0__ESAI_TX4_RX1 0x1b030
MX6QDL_PAD_ENET_MDC__ESAI_TX5_RX0 0x1b030
MX6QDL_PAD_GPIO_17__ESAI_TX0 0x1b030
MX6QDL_PAD_NANDF_CS3__ESAI_TX1 0x1b030
MX6QDL_PAD_ENET_MDIO__ESAI_RX_CLK 0x1b030
MX6QDL_PAD_GPIO_9__ESAI_RX_FS 0x1b030
>;
};
};
flexcan1 {
pinctrl_flexcan1_1: flexcan1grp-1 {
fsl,pins = <
MX6QDL_PAD_KEY_ROW2__FLEXCAN1_RX 0x80000000
MX6QDL_PAD_KEY_COL2__FLEXCAN1_TX 0x80000000
>;
};
pinctrl_flexcan1_2: flexcan1grp-2 {
fsl,pins = <
MX6QDL_PAD_GPIO_7__FLEXCAN1_TX 0x80000000
MX6QDL_PAD_KEY_ROW2__FLEXCAN1_RX 0x80000000
>;
};
};
flexcan2 {
pinctrl_flexcan2_1: flexcan2grp-1 {
fsl,pins = <
MX6QDL_PAD_KEY_COL4__FLEXCAN2_TX 0x80000000
MX6QDL_PAD_KEY_ROW4__FLEXCAN2_RX 0x80000000
>;
};
};
gpmi-nand {
pinctrl_gpmi_nand_1: gpmi-nand-1 {
fsl,pins = <
MX6QDL_PAD_NANDF_CLE__NAND_CLE 0xb0b1
MX6QDL_PAD_NANDF_ALE__NAND_ALE 0xb0b1
MX6QDL_PAD_NANDF_WP_B__NAND_WP_B 0xb0b1
MX6QDL_PAD_NANDF_RB0__NAND_READY_B 0xb000
MX6QDL_PAD_NANDF_CS0__NAND_CE0_B 0xb0b1
MX6QDL_PAD_NANDF_CS1__NAND_CE1_B 0xb0b1
MX6QDL_PAD_SD4_CMD__NAND_RE_B 0xb0b1
MX6QDL_PAD_SD4_CLK__NAND_WE_B 0xb0b1
MX6QDL_PAD_NANDF_D0__NAND_DATA00 0xb0b1
MX6QDL_PAD_NANDF_D1__NAND_DATA01 0xb0b1
MX6QDL_PAD_NANDF_D2__NAND_DATA02 0xb0b1
MX6QDL_PAD_NANDF_D3__NAND_DATA03 0xb0b1
MX6QDL_PAD_NANDF_D4__NAND_DATA04 0xb0b1
MX6QDL_PAD_NANDF_D5__NAND_DATA05 0xb0b1
MX6QDL_PAD_NANDF_D6__NAND_DATA06 0xb0b1
MX6QDL_PAD_NANDF_D7__NAND_DATA07 0xb0b1
MX6QDL_PAD_SD4_DAT0__NAND_DQS 0x00b1
>;
};
};
hdmi_hdcp {
pinctrl_hdmi_hdcp_1: hdmihdcpgrp-1 {
fsl,pins = <
MX6QDL_PAD_KEY_COL3__HDMI_TX_DDC_SCL 0x4001b8b1
MX6QDL_PAD_KEY_ROW3__HDMI_TX_DDC_SDA 0x4001b8b1
>;
};
pinctrl_hdmi_hdcp_2: hdmihdcpgrp-2 {
fsl,pins = <
MX6QDL_PAD_EIM_EB2__HDMI_TX_DDC_SCL 0x4001b8b1
MX6QDL_PAD_EIM_D16__HDMI_TX_DDC_SDA 0x4001b8b1
>;
};
pinctrl_hdmi_hdcp_3: hdmihdcpgrp-3 {
fsl,pins = <
MX6QDL_PAD_EIM_EB2__HDMI_TX_DDC_SCL 0x4001b8b1
MX6QDL_PAD_KEY_ROW3__HDMI_TX_DDC_SDA 0x4001b8b1
>;
};
};
hdmi_cec {
pinctrl_hdmi_cec_1: hdmicecgrp-1 {
fsl,pins = <
MX6QDL_PAD_EIM_A25__HDMI_TX_CEC_LINE 0x1f8b0
>;
};
pinctrl_hdmi_cec_2: hdmicecgrp-2 {
fsl,pins = <
MX6QDL_PAD_KEY_ROW2__HDMI_TX_CEC_LINE 0x1f8b0
>;
};
};
i2c1 {
pinctrl_i2c1_1: i2c1grp-1 {
fsl,pins = <
MX6QDL_PAD_EIM_D21__I2C1_SCL 0x4001b8b1
MX6QDL_PAD_EIM_D28__I2C1_SDA 0x4001b8b1
>;
};
pinctrl_i2c1_2: i2c1grp-2 {
fsl,pins = <
MX6QDL_PAD_CSI0_DAT8__I2C1_SDA 0x4001b8b1
MX6QDL_PAD_CSI0_DAT9__I2C1_SCL 0x4001b8b1
>;
};
};
i2c2 {
pinctrl_i2c2_1: i2c2grp-1 {
fsl,pins = <
MX6QDL_PAD_EIM_EB2__I2C2_SCL 0x4001b8b1
MX6QDL_PAD_EIM_D16__I2C2_SDA 0x4001b8b1
>;
};
pinctrl_i2c2_2: i2c2grp-2 {
fsl,pins = <
MX6QDL_PAD_KEY_COL3__I2C2_SCL 0x4001b8b1
MX6QDL_PAD_KEY_ROW3__I2C2_SDA 0x4001b8b1
>;
};
pinctrl_i2c2_3: i2c2grp-3 {
fsl,pins = <
MX6QDL_PAD_EIM_EB2__I2C2_SCL 0x4001b8b1
MX6QDL_PAD_KEY_ROW3__I2C2_SDA 0x4001b8b1
>;
};
};
i2c3 {
pinctrl_i2c3_1: i2c3grp-1 {
fsl,pins = <
MX6QDL_PAD_EIM_D17__I2C3_SCL 0x4001b8b1
MX6QDL_PAD_EIM_D18__I2C3_SDA 0x4001b8b1
>;
};
pinctrl_i2c3_2: i2c3grp-2 {
fsl,pins = <
MX6QDL_PAD_GPIO_3__I2C3_SCL 0x4001b8b1
MX6QDL_PAD_GPIO_6__I2C3_SDA 0x4001b8b1
>;
};
pinctrl_i2c3_3: i2c3grp-3 {
fsl,pins = <
MX6QDL_PAD_GPIO_5__I2C3_SCL 0x4001b8b1
MX6QDL_PAD_GPIO_16__I2C3_SDA 0x4001b8b1
>;
};
pinctrl_i2c3_4: i2c3grp-4 {
fsl,pins = <
MX6QDL_PAD_GPIO_3__I2C3_SCL 0x4001b8b1
MX6QDL_PAD_EIM_D18__I2C3_SDA 0x4001b8b1
>;
};
};
ipu1 {
pinctrl_ipu1_1: ipu1grp-1 {
fsl,pins = <
MX6QDL_PAD_DI0_DISP_CLK__IPU1_DI0_DISP_CLK 0x10
MX6QDL_PAD_DI0_PIN15__IPU1_DI0_PIN15 0x10
MX6QDL_PAD_DI0_PIN2__IPU1_DI0_PIN02 0x10
MX6QDL_PAD_DI0_PIN3__IPU1_DI0_PIN03 0x10
MX6QDL_PAD_DI0_PIN4__IPU1_DI0_PIN04 0x80000000
MX6QDL_PAD_DISP0_DAT0__IPU1_DISP0_DATA00 0x10
MX6QDL_PAD_DISP0_DAT1__IPU1_DISP0_DATA01 0x10
MX6QDL_PAD_DISP0_DAT2__IPU1_DISP0_DATA02 0x10
MX6QDL_PAD_DISP0_DAT3__IPU1_DISP0_DATA03 0x10
MX6QDL_PAD_DISP0_DAT4__IPU1_DISP0_DATA04 0x10
MX6QDL_PAD_DISP0_DAT5__IPU1_DISP0_DATA05 0x10
MX6QDL_PAD_DISP0_DAT6__IPU1_DISP0_DATA06 0x10
MX6QDL_PAD_DISP0_DAT7__IPU1_DISP0_DATA07 0x10
MX6QDL_PAD_DISP0_DAT8__IPU1_DISP0_DATA08 0x10
MX6QDL_PAD_DISP0_DAT9__IPU1_DISP0_DATA09 0x10
MX6QDL_PAD_DISP0_DAT10__IPU1_DISP0_DATA10 0x10
MX6QDL_PAD_DISP0_DAT11__IPU1_DISP0_DATA11 0x10
MX6QDL_PAD_DISP0_DAT12__IPU1_DISP0_DATA12 0x10
MX6QDL_PAD_DISP0_DAT13__IPU1_DISP0_DATA13 0x10
MX6QDL_PAD_DISP0_DAT14__IPU1_DISP0_DATA14 0x10
MX6QDL_PAD_DISP0_DAT15__IPU1_DISP0_DATA15 0x10
MX6QDL_PAD_DISP0_DAT16__IPU1_DISP0_DATA16 0x10
MX6QDL_PAD_DISP0_DAT17__IPU1_DISP0_DATA17 0x10
MX6QDL_PAD_DISP0_DAT18__IPU1_DISP0_DATA18 0x10
MX6QDL_PAD_DISP0_DAT19__IPU1_DISP0_DATA19 0x10
MX6QDL_PAD_DISP0_DAT20__IPU1_DISP0_DATA20 0x10
MX6QDL_PAD_DISP0_DAT21__IPU1_DISP0_DATA21 0x10
MX6QDL_PAD_DISP0_DAT22__IPU1_DISP0_DATA22 0x10
MX6QDL_PAD_DISP0_DAT23__IPU1_DISP0_DATA23 0x10
>;
};
pinctrl_ipu1_2: ipu1grp-2 { /* parallel camera */
fsl,pins = <
MX6QDL_PAD_CSI0_DAT12__IPU1_CSI0_DATA12 0x80000000
MX6QDL_PAD_CSI0_DAT13__IPU1_CSI0_DATA13 0x80000000
MX6QDL_PAD_CSI0_DAT14__IPU1_CSI0_DATA14 0x80000000
MX6QDL_PAD_CSI0_DAT15__IPU1_CSI0_DATA15 0x80000000
MX6QDL_PAD_CSI0_DAT16__IPU1_CSI0_DATA16 0x80000000
MX6QDL_PAD_CSI0_DAT17__IPU1_CSI0_DATA17 0x80000000
MX6QDL_PAD_CSI0_DAT18__IPU1_CSI0_DATA18 0x80000000
MX6QDL_PAD_CSI0_DAT19__IPU1_CSI0_DATA19 0x80000000
MX6QDL_PAD_CSI0_DATA_EN__IPU1_CSI0_DATA_EN 0x80000000
MX6QDL_PAD_CSI0_PIXCLK__IPU1_CSI0_PIXCLK 0x80000000
MX6QDL_PAD_CSI0_MCLK__IPU1_CSI0_HSYNC 0x80000000
MX6QDL_PAD_CSI0_VSYNC__IPU1_CSI0_VSYNC 0x80000000
>;
};
pinctrl_ipu1_3: ipu1grp-3 { /* parallel port 16-bit */
fsl,pins = <
MX6QDL_PAD_CSI0_DAT4__IPU1_CSI0_DATA04 0x80000000
MX6QDL_PAD_CSI0_DAT5__IPU1_CSI0_DATA05 0x80000000
MX6QDL_PAD_CSI0_DAT6__IPU1_CSI0_DATA06 0x80000000
MX6QDL_PAD_CSI0_DAT7__IPU1_CSI0_DATA07 0x80000000
MX6QDL_PAD_CSI0_DAT8__IPU1_CSI0_DATA08 0x80000000
MX6QDL_PAD_CSI0_DAT9__IPU1_CSI0_DATA09 0x80000000
MX6QDL_PAD_CSI0_DAT10__IPU1_CSI0_DATA10 0x80000000
MX6QDL_PAD_CSI0_DAT11__IPU1_CSI0_DATA11 0x80000000
MX6QDL_PAD_CSI0_DAT12__IPU1_CSI0_DATA12 0x80000000
MX6QDL_PAD_CSI0_DAT13__IPU1_CSI0_DATA13 0x80000000
MX6QDL_PAD_CSI0_DAT14__IPU1_CSI0_DATA14 0x80000000
MX6QDL_PAD_CSI0_DAT15__IPU1_CSI0_DATA15 0x80000000
MX6QDL_PAD_CSI0_DAT16__IPU1_CSI0_DATA16 0x80000000
MX6QDL_PAD_CSI0_DAT17__IPU1_CSI0_DATA17 0x80000000
MX6QDL_PAD_CSI0_DAT18__IPU1_CSI0_DATA18 0x80000000
MX6QDL_PAD_CSI0_DAT19__IPU1_CSI0_DATA19 0x80000000
MX6QDL_PAD_CSI0_PIXCLK__IPU1_CSI0_PIXCLK 0x80000000
MX6QDL_PAD_CSI0_MCLK__IPU1_CSI0_HSYNC 0x80000000
MX6QDL_PAD_CSI0_VSYNC__IPU1_CSI0_VSYNC 0x80000000
>;
};
};
mlb {
pinctrl_mlb_1: mlbgrp-1 {
fsl,pins = <
MX6QDL_PAD_GPIO_3__MLB_CLK 0x71
MX6QDL_PAD_GPIO_6__MLB_SIG 0x71
MX6QDL_PAD_GPIO_2__MLB_DATA 0x71
>;
};
pinctrl_mlb_2: mlbgrp-2 {
fsl,pins = <
MX6QDL_PAD_ENET_TXD1__MLB_CLK 0x71
MX6QDL_PAD_GPIO_6__MLB_SIG 0x71
MX6QDL_PAD_GPIO_2__MLB_DATA 0x71
>;
};
};
pwm0 {
pinctrl_pwm0_1: pwm0grp-1 {
fsl,pins = <
MX6QDL_PAD_SD1_DAT3__PWM1_OUT 0x1b0b1
>;
};
};
pwm3 {
pinctrl_pwm3_1: pwm3grp-1 {
fsl,pins = <
MX6QDL_PAD_SD4_DAT1__PWM3_OUT 0x1b0b1
>;
};
};
spdif {
pinctrl_spdif_1: spdifgrp-1 {
fsl,pins = <
MX6QDL_PAD_KEY_COL3__SPDIF_IN 0x1b0b0
>;
};
pinctrl_spdif_2: spdifgrp-2 {
fsl,pins = <
MX6QDL_PAD_GPIO_16__SPDIF_IN 0x1b0b0
MX6QDL_PAD_GPIO_17__SPDIF_OUT 0x1b0b0
>;
};
pinctrl_spdif_3: spdifgrp-3 {
fsl,pins = <
MX6QDL_PAD_ENET_RXD0__SPDIF_OUT 0x1b0b0
>;
};
};
uart1 {
pinctrl_uart1_1: uart1grp-1 {
fsl,pins = <
MX6QDL_PAD_CSI0_DAT10__UART1_TX_DATA 0x1b0b1
MX6QDL_PAD_CSI0_DAT11__UART1_RX_DATA 0x1b0b1
>;
};
};
uart2 {
pinctrl_uart2_1: uart2grp-1 {
fsl,pins = <
MX6QDL_PAD_EIM_D26__UART2_TX_DATA 0x1b0b1
MX6QDL_PAD_EIM_D27__UART2_RX_DATA 0x1b0b1
>;
};
pinctrl_uart2_2: uart2grp-2 { /* DTE mode */
fsl,pins = <
MX6QDL_PAD_EIM_D26__UART2_RX_DATA 0x1b0b1
MX6QDL_PAD_EIM_D27__UART2_TX_DATA 0x1b0b1
MX6QDL_PAD_EIM_D28__UART2_DTE_CTS_B 0x1b0b1
MX6QDL_PAD_EIM_D29__UART2_DTE_RTS_B 0x1b0b1
>;
};
};
uart3 {
pinctrl_uart3_1: uart3grp-1 {
fsl,pins = <
MX6QDL_PAD_SD4_CLK__UART3_RX_DATA 0x1b0b1
MX6QDL_PAD_SD4_CMD__UART3_TX_DATA 0x1b0b1
MX6QDL_PAD_EIM_D30__UART3_CTS_B 0x1b0b1
MX6QDL_PAD_EIM_EB3__UART3_RTS_B 0x1b0b1
>;
};
pinctrl_uart3_2: uart3grp-2 {
fsl,pins = <
MX6QDL_PAD_EIM_D24__UART3_TX_DATA 0x1b0b1
MX6QDL_PAD_EIM_D25__UART3_RX_DATA 0x1b0b1
MX6QDL_PAD_EIM_D23__UART3_CTS_B 0x1b0b1
MX6QDL_PAD_EIM_EB3__UART3_RTS_B 0x1b0b1
>;
};
};
uart4 {
pinctrl_uart4_1: uart4grp-1 {
fsl,pins = <
MX6QDL_PAD_KEY_COL0__UART4_TX_DATA 0x1b0b1
MX6QDL_PAD_KEY_ROW0__UART4_RX_DATA 0x1b0b1
>;
};
};
usbotg {
pinctrl_usbotg_1: usbotggrp-1 {
fsl,pins = <
MX6QDL_PAD_GPIO_1__USB_OTG_ID 0x17059
>;
};
pinctrl_usbotg_2: usbotggrp-2 {
fsl,pins = <
MX6QDL_PAD_ENET_RX_ER__USB_OTG_ID 0x17059
>;
};
};
usbh2 {
pinctrl_usbh2_1: usbh2grp-1 {
fsl,pins = <
MX6QDL_PAD_RGMII_TXC__USB_H2_DATA 0x40013030
MX6QDL_PAD_RGMII_TX_CTL__USB_H2_STROBE 0x40013030
>;
};
pinctrl_usbh2_2: usbh2grp-2 {
fsl,pins = <
MX6QDL_PAD_RGMII_TX_CTL__USB_H2_STROBE 0x40017030
>;
};
};
usbh3 {
pinctrl_usbh3_1: usbh3grp-1 {
fsl,pins = <
MX6QDL_PAD_RGMII_RX_CTL__USB_H3_DATA 0x40013030
MX6QDL_PAD_RGMII_RXC__USB_H3_STROBE 0x40013030
>;
};
pinctrl_usbh3_2: usbh3grp-2 {
fsl,pins = <
MX6QDL_PAD_RGMII_RXC__USB_H3_STROBE 0x40017030
>;
};
};
usdhc1 {
pinctrl_usdhc1_1: usdhc1grp-1 {
fsl,pins = <
MX6QDL_PAD_SD1_CMD__SD1_CMD 0x17059
MX6QDL_PAD_SD1_CLK__SD1_CLK 0x10059
MX6QDL_PAD_SD1_DAT0__SD1_DATA0 0x17059
MX6QDL_PAD_SD1_DAT1__SD1_DATA1 0x17059
MX6QDL_PAD_SD1_DAT2__SD1_DATA2 0x17059
MX6QDL_PAD_SD1_DAT3__SD1_DATA3 0x17059
MX6QDL_PAD_NANDF_D0__SD1_DATA4 0x17059
MX6QDL_PAD_NANDF_D1__SD1_DATA5 0x17059
MX6QDL_PAD_NANDF_D2__SD1_DATA6 0x17059
MX6QDL_PAD_NANDF_D3__SD1_DATA7 0x17059
>;
};
pinctrl_usdhc1_2: usdhc1grp-2 {
fsl,pins = <
MX6QDL_PAD_SD1_CMD__SD1_CMD 0x17059
MX6QDL_PAD_SD1_CLK__SD1_CLK 0x10059
MX6QDL_PAD_SD1_DAT0__SD1_DATA0 0x17059
MX6QDL_PAD_SD1_DAT1__SD1_DATA1 0x17059
MX6QDL_PAD_SD1_DAT2__SD1_DATA2 0x17059
MX6QDL_PAD_SD1_DAT3__SD1_DATA3 0x17059
>;
};
};
usdhc2 {
pinctrl_usdhc2_1: usdhc2grp-1 {
fsl,pins = <
MX6QDL_PAD_SD2_CMD__SD2_CMD 0x17059
MX6QDL_PAD_SD2_CLK__SD2_CLK 0x10059
MX6QDL_PAD_SD2_DAT0__SD2_DATA0 0x17059
MX6QDL_PAD_SD2_DAT1__SD2_DATA1 0x17059
MX6QDL_PAD_SD2_DAT2__SD2_DATA2 0x17059
MX6QDL_PAD_SD2_DAT3__SD2_DATA3 0x17059
MX6QDL_PAD_NANDF_D4__SD2_DATA4 0x17059
MX6QDL_PAD_NANDF_D5__SD2_DATA5 0x17059
MX6QDL_PAD_NANDF_D6__SD2_DATA6 0x17059
MX6QDL_PAD_NANDF_D7__SD2_DATA7 0x17059
>;
};
pinctrl_usdhc2_2: usdhc2grp-2 {
fsl,pins = <
MX6QDL_PAD_SD2_CMD__SD2_CMD 0x17059
MX6QDL_PAD_SD2_CLK__SD2_CLK 0x10059
MX6QDL_PAD_SD2_DAT0__SD2_DATA0 0x17059
MX6QDL_PAD_SD2_DAT1__SD2_DATA1 0x17059
MX6QDL_PAD_SD2_DAT2__SD2_DATA2 0x17059
MX6QDL_PAD_SD2_DAT3__SD2_DATA3 0x17059
>;
};
};
usdhc3 {
pinctrl_usdhc3_1: usdhc3grp-1 {
fsl,pins = <
MX6QDL_PAD_SD3_CMD__SD3_CMD 0x17059
MX6QDL_PAD_SD3_CLK__SD3_CLK 0x10059
MX6QDL_PAD_SD3_DAT0__SD3_DATA0 0x17059
MX6QDL_PAD_SD3_DAT1__SD3_DATA1 0x17059
MX6QDL_PAD_SD3_DAT2__SD3_DATA2 0x17059
MX6QDL_PAD_SD3_DAT3__SD3_DATA3 0x17059
MX6QDL_PAD_SD3_DAT4__SD3_DATA4 0x17059
MX6QDL_PAD_SD3_DAT5__SD3_DATA5 0x17059
MX6QDL_PAD_SD3_DAT6__SD3_DATA6 0x17059
MX6QDL_PAD_SD3_DAT7__SD3_DATA7 0x17059
>;
};
pinctrl_usdhc3_1_100mhz: usdhc3grp-1-100mhz { /* 100Mhz */
fsl,pins = <
MX6QDL_PAD_SD3_CMD__SD3_CMD 0x170b9
MX6QDL_PAD_SD3_CLK__SD3_CLK 0x100b9
MX6QDL_PAD_SD3_DAT0__SD3_DATA0 0x170b9
MX6QDL_PAD_SD3_DAT1__SD3_DATA1 0x170b9
MX6QDL_PAD_SD3_DAT2__SD3_DATA2 0x170b9
MX6QDL_PAD_SD3_DAT3__SD3_DATA3 0x170b9
MX6QDL_PAD_SD3_DAT4__SD3_DATA4 0x170b9
MX6QDL_PAD_SD3_DAT5__SD3_DATA5 0x170b9
MX6QDL_PAD_SD3_DAT6__SD3_DATA6 0x170b9
MX6QDL_PAD_SD3_DAT7__SD3_DATA7 0x170b9
>;
};
pinctrl_usdhc3_1_200mhz: usdhc3grp-1-200mhz { /* 200Mhz */
fsl,pins = <
MX6QDL_PAD_SD3_CMD__SD3_CMD 0x170f9
MX6QDL_PAD_SD3_CLK__SD3_CLK 0x100f9
MX6QDL_PAD_SD3_DAT0__SD3_DATA0 0x170f9
MX6QDL_PAD_SD3_DAT1__SD3_DATA1 0x170f9
MX6QDL_PAD_SD3_DAT2__SD3_DATA2 0x170f9
MX6QDL_PAD_SD3_DAT3__SD3_DATA3 0x170f9
MX6QDL_PAD_SD3_DAT4__SD3_DATA4 0x170f9
MX6QDL_PAD_SD3_DAT5__SD3_DATA5 0x170f9
MX6QDL_PAD_SD3_DAT6__SD3_DATA6 0x170f9
MX6QDL_PAD_SD3_DAT7__SD3_DATA7 0x170f9
>;
};
pinctrl_usdhc3_2: usdhc3grp-2 {
fsl,pins = <
MX6QDL_PAD_SD3_CMD__SD3_CMD 0x17059
MX6QDL_PAD_SD3_CLK__SD3_CLK 0x10059
MX6QDL_PAD_SD3_DAT0__SD3_DATA0 0x17059
MX6QDL_PAD_SD3_DAT1__SD3_DATA1 0x17059
MX6QDL_PAD_SD3_DAT2__SD3_DATA2 0x17059
MX6QDL_PAD_SD3_DAT3__SD3_DATA3 0x17059
>;
};
};
usdhc4 {
pinctrl_usdhc4_1: usdhc4grp-1 {
fsl,pins = <
MX6QDL_PAD_SD4_CMD__SD4_CMD 0x17059
MX6QDL_PAD_SD4_CLK__SD4_CLK 0x10059
MX6QDL_PAD_SD4_DAT0__SD4_DATA0 0x17059
MX6QDL_PAD_SD4_DAT1__SD4_DATA1 0x17059
MX6QDL_PAD_SD4_DAT2__SD4_DATA2 0x17059
MX6QDL_PAD_SD4_DAT3__SD4_DATA3 0x17059
MX6QDL_PAD_SD4_DAT4__SD4_DATA4 0x17059
MX6QDL_PAD_SD4_DAT5__SD4_DATA5 0x17059
MX6QDL_PAD_SD4_DAT6__SD4_DATA6 0x17059
MX6QDL_PAD_SD4_DAT7__SD4_DATA7 0x17059
>;
};
pinctrl_usdhc4_2: usdhc4grp-2 {
fsl,pins = <
MX6QDL_PAD_SD4_CMD__SD4_CMD 0x17059
MX6QDL_PAD_SD4_CLK__SD4_CLK 0x10059
MX6QDL_PAD_SD4_DAT0__SD4_DATA0 0x17059
MX6QDL_PAD_SD4_DAT1__SD4_DATA1 0x17059
MX6QDL_PAD_SD4_DAT2__SD4_DATA2 0x17059
MX6QDL_PAD_SD4_DAT3__SD4_DATA3 0x17059
>;
};
};
weim {
pinctrl_weim_cs0_1: weim_cs0grp-1 {
fsl,pins = <
MX6QDL_PAD_EIM_CS0__EIM_CS0_B 0xb0b1
>;
};
pinctrl_weim_nor_1: weim_norgrp-1 {
fsl,pins = <
MX6QDL_PAD_EIM_OE__EIM_OE_B 0xb0b1
MX6QDL_PAD_EIM_RW__EIM_RW 0xb0b1
MX6QDL_PAD_EIM_WAIT__EIM_WAIT_B 0xb060
/* data */
MX6QDL_PAD_EIM_D16__EIM_DATA16 0x1b0b0
MX6QDL_PAD_EIM_D17__EIM_DATA17 0x1b0b0
MX6QDL_PAD_EIM_D18__EIM_DATA18 0x1b0b0
MX6QDL_PAD_EIM_D19__EIM_DATA19 0x1b0b0
MX6QDL_PAD_EIM_D20__EIM_DATA20 0x1b0b0
MX6QDL_PAD_EIM_D21__EIM_DATA21 0x1b0b0
MX6QDL_PAD_EIM_D22__EIM_DATA22 0x1b0b0
MX6QDL_PAD_EIM_D23__EIM_DATA23 0x1b0b0
MX6QDL_PAD_EIM_D24__EIM_DATA24 0x1b0b0
MX6QDL_PAD_EIM_D25__EIM_DATA25 0x1b0b0
MX6QDL_PAD_EIM_D26__EIM_DATA26 0x1b0b0
MX6QDL_PAD_EIM_D27__EIM_DATA27 0x1b0b0
MX6QDL_PAD_EIM_D28__EIM_DATA28 0x1b0b0
MX6QDL_PAD_EIM_D29__EIM_DATA29 0x1b0b0
MX6QDL_PAD_EIM_D30__EIM_DATA30 0x1b0b0
MX6QDL_PAD_EIM_D31__EIM_DATA31 0x1b0b0
/* address */
MX6QDL_PAD_EIM_A23__EIM_ADDR23 0xb0b1
MX6QDL_PAD_EIM_A22__EIM_ADDR22 0xb0b1
MX6QDL_PAD_EIM_A21__EIM_ADDR21 0xb0b1
MX6QDL_PAD_EIM_A20__EIM_ADDR20 0xb0b1
MX6QDL_PAD_EIM_A19__EIM_ADDR19 0xb0b1
MX6QDL_PAD_EIM_A18__EIM_ADDR18 0xb0b1
MX6QDL_PAD_EIM_A17__EIM_ADDR17 0xb0b1
MX6QDL_PAD_EIM_A16__EIM_ADDR16 0xb0b1
MX6QDL_PAD_EIM_DA15__EIM_AD15 0xb0b1
MX6QDL_PAD_EIM_DA14__EIM_AD14 0xb0b1
MX6QDL_PAD_EIM_DA13__EIM_AD13 0xb0b1
MX6QDL_PAD_EIM_DA12__EIM_AD12 0xb0b1
MX6QDL_PAD_EIM_DA11__EIM_AD11 0xb0b1
MX6QDL_PAD_EIM_DA10__EIM_AD10 0xb0b1
MX6QDL_PAD_EIM_DA9__EIM_AD09 0xb0b1
MX6QDL_PAD_EIM_DA8__EIM_AD08 0xb0b1
MX6QDL_PAD_EIM_DA7__EIM_AD07 0xb0b1
MX6QDL_PAD_EIM_DA6__EIM_AD06 0xb0b1
MX6QDL_PAD_EIM_DA5__EIM_AD05 0xb0b1
MX6QDL_PAD_EIM_DA4__EIM_AD04 0xb0b1
MX6QDL_PAD_EIM_DA3__EIM_AD03 0xb0b1
MX6QDL_PAD_EIM_DA2__EIM_AD02 0xb0b1
MX6QDL_PAD_EIM_DA1__EIM_AD01 0xb0b1
MX6QDL_PAD_EIM_DA0__EIM_AD00 0xb0b1
>;
};
};
};
ldb: ldb@020e0008 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6q-ldb", "fsl,imx53-ldb";
gpr = <&gpr>;
status = "disabled";
lvds-channel@0 {
reg = <0>;
status = "disabled";
};
lvds-channel@1 {
reg = <1>;
status = "disabled";
};
};
dcic1: dcic@020e4000 {
reg = <0x020e4000 0x4000>;
interrupts = <0 124 0x04>;
};
dcic2: dcic@020e8000 {
reg = <0x020e8000 0x4000>;
interrupts = <0 125 0x04>;
};
sdma: sdma@020ec000 {
compatible = "fsl,imx6q-sdma", "fsl,imx35-sdma";
reg = <0x020ec000 0x4000>;
interrupts = <0 2 0x04>;
clocks = <&clks 155>, <&clks 155>;
clock-names = "ipg", "ahb";
#dma-cells = <3>;
fsl,sdma-ram-script-name = "imx/sdma/sdma-imx6q.bin";
};
};
aips-bus@02100000 { /* AIPS2 */
compatible = "fsl,aips-bus", "simple-bus";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x02100000 0x100000>;
ranges;
caam@02100000 {
reg = <0x02100000 0x40000>;
interrupts = <0 105 0x04 0 106 0x04>;
};
aipstz@0217c000 { /* AIPSTZ2 */
reg = <0x0217c000 0x4000>;
};
usbotg: usb@02184000 {
compatible = "fsl,imx6q-usb", "fsl,imx27-usb";
reg = <0x02184000 0x200>;
interrupts = <0 43 0x04>;
clocks = <&clks 162>;
fsl,usbphy = <&usbphy1>;
fsl,usbmisc = <&usbmisc 0>;
status = "disabled";
};
usbh1: usb@02184200 {
compatible = "fsl,imx6q-usb", "fsl,imx27-usb";
reg = <0x02184200 0x200>;
interrupts = <0 40 0x04>;
clocks = <&clks 162>;
fsl,usbphy = <&usbphy2>;
fsl,usbmisc = <&usbmisc 1>;
status = "disabled";
};
usbh2: usb@02184400 {
compatible = "fsl,imx6q-usb", "fsl,imx27-usb";
reg = <0x02184400 0x200>;
interrupts = <0 41 0x04>;
clocks = <&clks 162>;
fsl,usbmisc = <&usbmisc 2>;
status = "disabled";
};
usbh3: usb@02184600 {
compatible = "fsl,imx6q-usb", "fsl,imx27-usb";
reg = <0x02184600 0x200>;
interrupts = <0 42 0x04>;
clocks = <&clks 162>;
fsl,usbmisc = <&usbmisc 3>;
status = "disabled";
};
usbmisc: usbmisc@02184800 {
#index-cells = <1>;
compatible = "fsl,imx6q-usbmisc";
reg = <0x02184800 0x200>;
clocks = <&clks 162>;
};
fec: ethernet@02188000 {
compatible = "fsl,imx6q-fec";
reg = <0x02188000 0x4000>;
interrupts = <0 118 0x04 0 119 0x04>;
clocks = <&clks 117>, <&clks 117>, <&clks 190>;
clock-names = "ipg", "ahb", "ptp";
status = "disabled";
};
mlb@0218c000 {
reg = <0x0218c000 0x4000>;
interrupts = <0 53 0x04 0 117 0x04 0 126 0x04>;
};
usdhc1: usdhc@02190000 {
compatible = "fsl,imx6q-usdhc";
reg = <0x02190000 0x4000>;
interrupts = <0 22 0x04>;
clocks = <&clks 163>, <&clks 163>, <&clks 163>;
clock-names = "ipg", "ahb", "per";
bus-width = <4>;
status = "disabled";
};
usdhc2: usdhc@02194000 {
compatible = "fsl,imx6q-usdhc";
reg = <0x02194000 0x4000>;
interrupts = <0 23 0x04>;
clocks = <&clks 164>, <&clks 164>, <&clks 164>;
clock-names = "ipg", "ahb", "per";
bus-width = <4>;
status = "disabled";
};
usdhc3: usdhc@02198000 {
compatible = "fsl,imx6q-usdhc";
reg = <0x02198000 0x4000>;
interrupts = <0 24 0x04>;
clocks = <&clks 165>, <&clks 165>, <&clks 165>;
clock-names = "ipg", "ahb", "per";
bus-width = <4>;
status = "disabled";
};
usdhc4: usdhc@0219c000 {
compatible = "fsl,imx6q-usdhc";
reg = <0x0219c000 0x4000>;
interrupts = <0 25 0x04>;
clocks = <&clks 166>, <&clks 166>, <&clks 166>;
clock-names = "ipg", "ahb", "per";
bus-width = <4>;
status = "disabled";
};
i2c1: i2c@021a0000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6q-i2c", "fsl,imx21-i2c";
reg = <0x021a0000 0x4000>;
interrupts = <0 36 0x04>;
clocks = <&clks 125>;
status = "disabled";
};
i2c2: i2c@021a4000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6q-i2c", "fsl,imx21-i2c";
reg = <0x021a4000 0x4000>;
interrupts = <0 37 0x04>;
clocks = <&clks 126>;
status = "disabled";
};
i2c3: i2c@021a8000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6q-i2c", "fsl,imx21-i2c";
reg = <0x021a8000 0x4000>;
interrupts = <0 38 0x04>;
clocks = <&clks 127>;
status = "disabled";
};
romcp@021ac000 {
reg = <0x021ac000 0x4000>;
};
/*mmdc0: mmdc@021b0000 {
compatible = "fsl,imx6q-mmdc";
reg = <0x021b0000 0x4000>;
};
mmdc1: mmdc@021b4000 {
reg = <0x021b4000 0x4000>;
};*/
weim: weim@021b8000 {
compatible = "fsl,imx6q-weim";
reg = <0x021b8000 0x4000>;
interrupts = <0 14 0x04>;
clocks = <&clks 196>;
};
/*ocotp: ocotp@021bc000 {
compatible = "fsl,imx6q-ocotp", "syscon";
reg = <0x021bc000 0x4000>;
};*/
tzasc@021d0000 { /* TZASC1 */
reg = <0x021d0000 0x4000>;
interrupts = <0 108 0x04>;
};
tzasc@021d4000 { /* TZASC2 */
reg = <0x021d4000 0x4000>;
interrupts = <0 109 0x04>;
};
audmux: audmux@021d8000 {
compatible = "fsl,imx6q-audmux", "fsl,imx31-audmux";
reg = <0x021d8000 0x4000>;
status = "disabled";
};
mipi@021dc000 { /* MIPI-CSI */
reg = <0x021dc000 0x4000>;
};
mipi@021e0000 { /* MIPI-DSI */
reg = <0x021e0000 0x4000>;
};
vdoa@021e4000 {
reg = <0x021e4000 0x4000>;
interrupts = <0 18 0x04>;
};
uart2: serial@021e8000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x021e8000 0x4000>;
interrupts = <0 27 0x04>;
clocks = <&clks 160>, <&clks 161>;
clock-names = "ipg", "per";
dmas = <&sdma 27 4 0>, <&sdma 28 4 0>;
dma-names = "rx", "tx";
status = "disabled";
};
uart3: serial@021ec000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x021ec000 0x4000>;
interrupts = <0 28 0x04>;
clocks = <&clks 160>, <&clks 161>;
clock-names = "ipg", "per";
dmas = <&sdma 29 4 0>, <&sdma 30 4 0>;
dma-names = "rx", "tx";
status = "disabled";
};
uart4: serial@021f0000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x021f0000 0x4000>;
interrupts = <0 29 0x04>;
clocks = <&clks 160>, <&clks 161>;
clock-names = "ipg", "per";
dmas = <&sdma 31 4 0>, <&sdma 32 4 0>;
dma-names = "rx", "tx";
status = "disabled";
};
uart5: serial@021f4000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x021f4000 0x4000>;
interrupts = <0 30 0x04>;
clocks = <&clks 160>, <&clks 161>;
clock-names = "ipg", "per";
dmas = <&sdma 33 4 0>, <&sdma 34 4 0>;
dma-names = "rx", "tx";
status = "disabled";
};
};
ipu1: ipu@02400000 {
#crtc-cells = <1>;
compatible = "fsl,imx6q-ipu";
reg = <0x02400000 0x400000>;
interrupts = <0 6 0x4 0 5 0x4>;
clocks = <&clks 130>, <&clks 131>, <&clks 132>;
clock-names = "bus", "di0", "di1";
resets = <&src 2>;
};
};
};
Regards
Prethibha