Driving odd LED/LCD panel formats

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Driving odd LED/LCD panel formats

1,938件の閲覧回数
chrisrayner
Contributor I

I am looking to drive odd panel formats with the i.MX8M - 1:1, 4:1 and 5.3:1 aspect ratios. Is there the capability to drive these formats and adjust the mipi output with a dumb LVDS converter (aka TI's SN65DSI84) to drive a panel directly or would I need an iumage converter like the Lattice SiliconImage series of devices?

0 件の賞賛
返信
1 返信

1,473件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chris

one can look at MIPI DSI panel driver for rm67191, which gives timing data without edid.

Adjust lcd timings in "struct display_timing rad_default_timing"
drivers\gpu\drm\panel\panel-raydium-rm67191.c

panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel 

sn65dsi85 example :

how to use ldb/lvds in android8 of imx8mq ? 

boundary devices lcd settings:

Yocto release for i.MX 8MQ - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信