It is mentioned on the NXP website that Silex is a proven partner (NXP - Partner Profile Information ). One of the supported devices is the SX-PCEAC2 WiFi module with QCA6174-5 chip. Two questions:
Hi Hans
it is supported in NXP Linux 4.9.88, one can look in Linux Manual included in
Linux 4.9.88_2.0.0 BSP & Multimedia Codecs Documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
This is a bit confusing:
- the documentation that you are referring to is about the QCA CLD driver
- in the article How to evaluate QCA6174 radio on i.MX 8 EVK platform?, the ath10k driver is used.
These aren't the same drivers. NXP supports the same chip with different drivers ?
Best regards,
Hans
Hi Hans
below part of L4.9.88_2.0.0 Release Notes
could you point where in official documentation "QCA CLD driver" mentioned.
May be also useful to check murata wifi imx portal:
wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html
Article is just another solution, note nxp official documents are located on
Best regards
igor