How to evaluate QCA6174 radio on i.MX 8 EVK platform?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to evaluate QCA6174 radio on i.MX 8 EVK platform?

Jump to solution
1,229 Views
babarhashim
Contributor III

Step by step instructions to how to begin your evaluation for the QCA6174 radio module, the SX-PCEAC2, on the i.MX 8 EVK.

Tags (1)
0 Kudos
Reply
1 Solution
969 Views
babarhashim
Contributor III

The SX-PCEAC2 is powered by Qualcomm Atheros QCA6174-5 radio chip, which features 2x2 wave 2 MU-MIMO technology. It is a dual-band 802.11 a/b/g/n/ac module with Bluetooth support which is designed for devices that require wireless connectivity in a small form factor combined with high performance. The SX-PCEAC2 comes in a half mini-card form-factor that allows customers to easily evaluate the radio with the i.MX 8 with either the NXP provided BSP or the Silex evaluation image. 

1. Use the NXP BSP:

The NXP i.MX8M ships with the Linux BSP that uses the WLAN ath10k driver. The board data file used is not optimized for best performance for both the on-board radio and the Silex’s SX-PCEAC2. But it does work and is the quickest way to evaluation (Not recommended for evaluation for performance and mass production purposes). 

 

2. Use the Silex Evaluation Image (RECOMMENDED):

Silex offers an evaluation image that uses the ath10k WLAN driver and has the following advantages

  • Includes tools to test basic wireless functionality, wireless security and data throughput
  • Includes the optimized board data file needed to leverage the Silex's modular certification
  • Enables "AP Mode" functionality

Platform Specifics

Platform

NXP i.MX8M Development Board (MCIMX8M-EVK)

Operating System

Linux BSP Version L4.9.51_8MQ_GA

Wi-Fi Driver

ath10k (open source)

 

What you will need?

SX-PCEAC2-EVK
NXP i.MX8M Development Board (MCIMX8M-EVK)
8GB SDHC Flash Card (Only required for Silex evaluation image) 

You will also need the evaluation software and the step by step instructions in the user guide.

How to Evaluate Video Tutorial: 

This short video provides step by step instructions to how to begin your evaluation.

View solution in original post

0 Kudos
Reply
1 Reply
970 Views
babarhashim
Contributor III

The SX-PCEAC2 is powered by Qualcomm Atheros QCA6174-5 radio chip, which features 2x2 wave 2 MU-MIMO technology. It is a dual-band 802.11 a/b/g/n/ac module with Bluetooth support which is designed for devices that require wireless connectivity in a small form factor combined with high performance. The SX-PCEAC2 comes in a half mini-card form-factor that allows customers to easily evaluate the radio with the i.MX 8 with either the NXP provided BSP or the Silex evaluation image. 

1. Use the NXP BSP:

The NXP i.MX8M ships with the Linux BSP that uses the WLAN ath10k driver. The board data file used is not optimized for best performance for both the on-board radio and the Silex’s SX-PCEAC2. But it does work and is the quickest way to evaluation (Not recommended for evaluation for performance and mass production purposes). 

 

2. Use the Silex Evaluation Image (RECOMMENDED):

Silex offers an evaluation image that uses the ath10k WLAN driver and has the following advantages

  • Includes tools to test basic wireless functionality, wireless security and data throughput
  • Includes the optimized board data file needed to leverage the Silex's modular certification
  • Enables "AP Mode" functionality

Platform Specifics

Platform

NXP i.MX8M Development Board (MCIMX8M-EVK)

Operating System

Linux BSP Version L4.9.51_8MQ_GA

Wi-Fi Driver

ath10k (open source)

 

What you will need?

SX-PCEAC2-EVK
NXP i.MX8M Development Board (MCIMX8M-EVK)
8GB SDHC Flash Card (Only required for Silex evaluation image) 

You will also need the evaluation software and the step by step instructions in the user guide.

How to Evaluate Video Tutorial: 

This short video provides step by step instructions to how to begin your evaluation.

0 Kudos
Reply