Driver for QCA6174 and support for i.MX7 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Driver for QCA6174 and support for i.MX7 ?

1,192 Views
hvparys
Contributor III

It is mentioned on the NXP website that Silex is a proven partner (NXP - Partner Profile Information ). One of the supported devices is the SX-PCEAC2 WiFi module with QCA6174-5 chip. Two questions:

  1. Can you specify what driver is used for this device ?
  2. Why are most i.MX6 and i.MX8 devices mentioned in the list of processors that support it, but not the i.MX7 ?
Tags (2)
0 Kudos
Reply
4 Replies

968 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hans

it is supported in NXP Linux 4.9.88, one can look in Linux Manual included in

Linux 4.9.88_2.0.0 BSP & Multimedia Codecs Documentation

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

968 Views
hvparys
Contributor III

Hi Igor,

This is a bit confusing:

- the documentation that you are referring to is about the QCA CLD driver

- in the article How to evaluate QCA6174 radio on i.MX 8 EVK platform?, the ath10k driver is used.

These aren't the same drivers. NXP supports the same chip with different drivers ?

Best regards,

Hans

0 Kudos
Reply

968 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hans

below part of L4.9.88_2.0.0 Release Notes

pastedImage_2.jpg

could you point where in official documentation "QCA CLD driver" mentioned.

May be also useful to check murata wifi imx portal:

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Article is just another solution, note nxp official documents are located on

i.MX Software|NXP 

Best regards
igor

0 Kudos
Reply

968 Views
hvparys
Contributor III

Hi Igor,

QCA CLD is mentioned in the i.MX Reference Manual (Document IMXLXRM, Rev. L.4.9.88_2.0.0-ga, 05/2018), section 4.12.2.

Best regards,

Hans

0 Kudos
Reply