mxsldr and mxsboot for imx7 chipsets

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mxsldr and mxsboot for imx7 chipsets

649 Views
sonu_abraham
Contributor I

Hi All,

I have the following two questions regarding imx7 chipsets

1) Is it possible to use mxsldr and mxsboot tools to provision a bare board with u-boot , kernel and rootfs ? Is the two tools supported for imx7 boards ?

2) Is is possible to download download u-boot, kernel and rootfs to QSPI flash devices if the mxsldr and mxsboot tools are supported for the imx7 processors.

Thanks in advance,

Sonu Abraham

Labels (3)
Tags (3)
0 Kudos
Reply
1 Reply

552 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sonu

unfortunately mxsldr and mxsboot tools are not suppoted by nxp,

for image programming is used mfg tool utility found on

i.MX Software|NXP 

In general yes, it is possible to download download u-boot, kernel and rootfs to QSPI flash

if its size allows for it.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply