Does the i.MX8MP have an Secondary Memory Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the i.MX8MP have an Secondary Memory Interface

Jump to solution
3,383 Views
HankChang989
Contributor II
0 Kudos
Reply
1 Solution
3,350 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HankChang989 ,

I hope you are doing well.

->There is no support imx8mplus gives for a secondary memory interface as Raspberry has.
->SMI offers a very fast parallel interface - over 80 megabytes per second on a ZeroW.

->The external memory interface on the i.MX precisely seems the Raspberry Pi's "Secondary Memory Interface". So it's good to use it there is equivalent functionality.
->Using the external memory interface gives better performance and more flexibility about the timings.
->Imx8m plus gives LPDDR4, DDR4 (32-bit up to 4.0GT/s)external memory interface support.

->One can find more features about imx8mp in the below-given link.
https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

I hope this information helps you!

Thanks & Regards,

Sanket Parekh

View solution in original post

6 Replies
3,351 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HankChang989 ,

I hope you are doing well.

->There is no support imx8mplus gives for a secondary memory interface as Raspberry has.
->SMI offers a very fast parallel interface - over 80 megabytes per second on a ZeroW.

->The external memory interface on the i.MX precisely seems the Raspberry Pi's "Secondary Memory Interface". So it's good to use it there is equivalent functionality.
->Using the external memory interface gives better performance and more flexibility about the timings.
->Imx8m plus gives LPDDR4, DDR4 (32-bit up to 4.0GT/s)external memory interface support.

->One can find more features about imx8mp in the below-given link.
https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

I hope this information helps you!

Thanks & Regards,

Sanket Parekh

3,346 Views
HankChang989
Contributor II

Thank you Snaket Parekh for the prompt response.

1.What is the bit width of the Parallel bus address and data? (Are both the address and data 32-bit?)

2.Is there any sample code available for reference?

3.I want to control the timing of 0 and 1 for data bit, is it possible? 

HankChang989_0-1682486412111.png

 

0 Kudos
Reply
3,318 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HankChang989 ,

I hope you are doing well.

1. What is the bit width of the Parallel bus address and data? (Are both the address and data 32-bit?)
->It is not fixed because the programmable Data port sizes for each Chip Select are x8, x16, and x32.
->There is Independent synchronous Memory Burst Read Mode support for NOR-Flash and PSRAM memories like x16 and x32 port size.

About this one can refer to SRAM.
->EIM gives support for multiplexed address/data bus operation x16 and x32 port sizes.

2. Is there any sample code available for reference?
3. I want to control the timing of 0 and 1 for the data bit, is it possible?
->Please kindly share the details about these queries.

Thanks & Regards,
Sanket Parekh
3,288 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HankChang989 

 

I hope you are doing well.

Any Updates from your side?

 

Thanks & Regards,

Sanket Parekh

3,270 Views
HankChang989
Contributor II

Thank you for your quick response and following up on the issue.

The issue has been resolved. Thank you for your assistance.

Have a great day!

0 Kudos
Reply
3,248 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HankChang989 ,

I hope you are doing well.

I'm glad that the issue is resolved.
Hence closing this case.

Have a great day!

Thanks & Regards,

Sanket Parekh