Does the i.MX8MP have an Secondary Memory Interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does the i.MX8MP have an Secondary Memory Interface

跳至解决方案
3,386 次查看
HankChang989
Contributor II
0 项奖励
回复
1 解答
3,353 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HankChang989 ,

I hope you are doing well.

->There is no support imx8mplus gives for a secondary memory interface as Raspberry has.
->SMI offers a very fast parallel interface - over 80 megabytes per second on a ZeroW.

->The external memory interface on the i.MX precisely seems the Raspberry Pi's "Secondary Memory Interface". So it's good to use it there is equivalent functionality.
->Using the external memory interface gives better performance and more flexibility about the timings.
->Imx8m plus gives LPDDR4, DDR4 (32-bit up to 4.0GT/s)external memory interface support.

->One can find more features about imx8mp in the below-given link.
https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

I hope this information helps you!

Thanks & Regards,

Sanket Parekh

在原帖中查看解决方案

6 回复数
3,354 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HankChang989 ,

I hope you are doing well.

->There is no support imx8mplus gives for a secondary memory interface as Raspberry has.
->SMI offers a very fast parallel interface - over 80 megabytes per second on a ZeroW.

->The external memory interface on the i.MX precisely seems the Raspberry Pi's "Secondary Memory Interface". So it's good to use it there is equivalent functionality.
->Using the external memory interface gives better performance and more flexibility about the timings.
->Imx8m plus gives LPDDR4, DDR4 (32-bit up to 4.0GT/s)external memory interface support.

->One can find more features about imx8mp in the below-given link.
https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

I hope this information helps you!

Thanks & Regards,

Sanket Parekh

3,349 次查看
HankChang989
Contributor II

Thank you Snaket Parekh for the prompt response.

1.What is the bit width of the Parallel bus address and data? (Are both the address and data 32-bit?)

2.Is there any sample code available for reference?

3.I want to control the timing of 0 and 1 for data bit, is it possible? 

HankChang989_0-1682486412111.png

 

0 项奖励
回复
3,321 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HankChang989 ,

I hope you are doing well.

1. What is the bit width of the Parallel bus address and data? (Are both the address and data 32-bit?)
->It is not fixed because the programmable Data port sizes for each Chip Select are x8, x16, and x32.
->There is Independent synchronous Memory Burst Read Mode support for NOR-Flash and PSRAM memories like x16 and x32 port size.

About this one can refer to SRAM.
->EIM gives support for multiplexed address/data bus operation x16 and x32 port sizes.

2. Is there any sample code available for reference?
3. I want to control the timing of 0 and 1 for the data bit, is it possible?
->Please kindly share the details about these queries.

Thanks & Regards,
Sanket Parekh
3,291 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HankChang989 

 

I hope you are doing well.

Any Updates from your side?

 

Thanks & Regards,

Sanket Parekh

3,273 次查看
HankChang989
Contributor II

Thank you for your quick response and following up on the issue.

The issue has been resolved. Thank you for your assistance.

Have a great day!

0 项奖励
回复
3,251 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @HankChang989 ,

I hope you are doing well.

I'm glad that the issue is resolved.
Hence closing this case.

Have a great day!

Thanks & Regards,

Sanket Parekh