Does imx6sololite with GPU support OPEN CL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does imx6sololite with GPU support OPEN CL

1,720件の閲覧回数
fisherhe
Contributor II

Hi,

    Does imx6 sololite with GPU,like MCIMX6L3DVN10AB ,support OPEN CL? If the answer is YES, which version of OPEN CL does it support?

     I know IMX6Q support OPEN CL, but the GPU of IMX6L3D seems not the same as IMX6S/D/Q. I don't know if IMX6L3D support OPEN CL or not. Are there any technique docements?

     Thanks.

2 返答(返信)

1,641件の閲覧回数
mtx512
Contributor V

I would verify that MCIMX6L3DVN10AB actually has 3D support because datasheet indicates 2D + OpenVG only. Therefore no Open CL, furthermore beware on most i.mx6 processors Open CL is restricted to the EP (Embedded Profile) which severely limits its capabilities.  

1,641件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

In the newest linux BSP, details you can see in document i.MX_Linux_Release_Notes.

opencl support.PNG

Hope this can do help for you.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信