Does imx6sololite with GPU support OPEN CL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does imx6sololite with GPU support OPEN CL

1,719 Views
fisherhe
Contributor II

Hi,

    Does imx6 sololite with GPU,like MCIMX6L3DVN10AB ,support OPEN CL? If the answer is YES, which version of OPEN CL does it support?

     I know IMX6Q support OPEN CL, but the GPU of IMX6L3D seems not the same as IMX6S/D/Q. I don't know if IMX6L3D support OPEN CL or not. Are there any technique docements?

     Thanks.

2 Replies

1,640 Views
mtx512
Contributor V

I would verify that MCIMX6L3DVN10AB actually has 3D support because datasheet indicates 2D + OpenVG only. Therefore no Open CL, furthermore beware on most i.mx6 processors Open CL is restricted to the EP (Embedded Profile) which severely limits its capabilities.  

1,640 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

In the newest linux BSP, details you can see in document i.MX_Linux_Release_Notes.

opencl support.PNG

Hope this can do help for you.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply