Hi,community:
my device is i.mx6q+android 4.4.2, I write an simple android app to play video with android api videoview. I found my device can play sdcard video and udp multicast video, but can't play udp unicast stream. Test video's format is H264, and the steamming source is VLC on pc.
Android app like this:
VideoView videoView = (MyView)findViewById(R.id.videoview1);
Uri uri =Uri.parse("udp://10.14.25.3:1234");
videoView.setVideoURI(uri);
videoView.start();
Device IP is 10.14.25.3, and udp port is 1234, when playing udp unicast video, logcat always print Reconnecting, and if I input tcpdump in shell , I can see this, so the net is ok.
root@sabresd_6dq:/tcpdump -c 1 -t udp port 1234
listening on eth0, link-type EN10MB (Ethernet), capture size 96 bytes
IP 10.14.0.2.50672 > 10.14.25.3.1234: UDP, length 1316
1 packets captured
2 packets received by filter
0 packets dropped by kernel
Here is udp unicast logcat:
10-31 17:50:45.210 I/OMXPlayer( 3561): LEVEL: 1 FUNCTION: prepare LINE: 528
10-31 17:50:45.210 I/OMXPlayer( 3561): failed to open file: /data/system/audio_pass_through_pref.
10-31 17:50:45.210 I/OMXPlayer( 3561): Loading content: udp://10.14.25.3:123410-31 17:50:45.380 I/OMXPlayer( 2453): Reconnecting...
10-31 17:50:47.580 I/OMXPlayer( 2453): Reconnecting...
10-31 17:50:49.790 I/OMXPlayer( 2453): Reconnecting...
10-31 17:50:51.990 I/OMXPlayer( 2453): Reconnecting...
Can any help me? Thank you!
已解决! 转到解答。
Here is a document regarding to setup multicast for Android on i.MX6:
https://community.nxp.com/docs/DOC-100045