Does i.MX6Q+android4.4.2 support playing udp unicast?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does i.MX6Q+android4.4.2 support playing udp unicast?

跳至解决方案
1,709 次查看
lqll
Contributor III

Hi,community:

   my device is i.mx6q+android 4.4.2, I write an simple android app to play video with android api videoview. I found my device can play sdcard video and udp multicast video, but can't play udp unicast stream. Test video's format is H264, and the steamming source is VLC on pc.

   Android app like this:

VideoView videoView = (MyView)findViewById(R.id.videoview1);

Uri uri =Uri.parse("udp://10.14.25.3:1234");
videoView.setVideoURI(uri);
videoView.start();

   Device IP is 10.14.25.3, and udp port is 1234, when playing udp unicast video, logcat always print Reconnecting, and if I input tcpdump in shell , I can see this, so the net is ok.

root@sabresd_6dq:/tcpdump -c 1 -t udp port 1234

listening on eth0, link-type EN10MB (Ethernet), capture size 96 bytes
IP 10.14.0.2.50672 > 10.14.25.3.1234: UDP, length 1316
1 packets captured
2 packets received by filter
0 packets dropped by kernel

Here is udp unicast logcat:

10-31 17:50:45.210 I/OMXPlayer( 3561): LEVEL: 1 FUNCTION: prepare LINE: 528
10-31 17:50:45.210 I/OMXPlayer( 3561): failed to open file: /data/system/audio_pass_through_pref.
10-31 17:50:45.210 I/OMXPlayer( 3561): Loading content: udp://10.14.25.3:1234

10-31 17:50:45.380 I/OMXPlayer( 2453): Reconnecting...
10-31 17:50:47.580 I/OMXPlayer( 2453): Reconnecting...
10-31 17:50:49.790 I/OMXPlayer( 2453): Reconnecting...
10-31 17:50:51.990 I/OMXPlayer( 2453): Reconnecting...

Can any help me? Thank you!

标签 (2)
0 项奖励
回复
1 解答
1,605 次查看
b36401
NXP Employee
NXP Employee

Here is a document regarding to setup multicast for Android on i.MX6:
https://community.nxp.com/docs/DOC-100045

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,606 次查看
b36401
NXP Employee
NXP Employee

Here is a document regarding to setup multicast for Android on i.MX6:
https://community.nxp.com/docs/DOC-100045

0 项奖励
回复