Does enabling Secure Boot in the RT600 family make it unusable in other devices?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does enabling Secure Boot in the RT600 family make it unusable in other devices?

ソリューションへジャンプ
1,146件の閲覧回数
hxp123
Contributor II

I have a device that is running an RT600 family MCU. I'd like to make a custom development board and I'm curious if I can re-use that RT600 or not.

I believe secureboot is enabled on this RT600, and - as I currently understand it - enabling secure boot sets OTP fuses which will make my custom dev board firmware not be accepted by the MCU.

Is my understanding about this correct? Does enabling secureboot prevent it from being used with any firmware not signed by the original private key?

 

thank you

ラベル(1)
0 件の賞賛
返信
1 解決策
1,132件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @hxp123 ,

   Your understanding is correct.

  If you do the secure boot, then you also need to prepare the related secure app firmware to match it, and download to the flash, then it will be used correctly.

  If just normal app without the related secure configuration, can't be boot any more, as it lack the sign or secured information.

  More details, please refer to the user manual secure chapter, and our tools: SPT and the MCUbootutlity:

1. SPT

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-s...

 

2. MCUbootutility

https://github.com/JayHeng/NXP-MCUBootUtility/releases/tag/v5.3.0
the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility

 

Wish it helps you!

Best Regards,

Kerry

 

元の投稿で解決策を見る

2 返答(返信)
1,128件の閲覧回数
hxp123
Contributor II

Hi Kerry, thank you so much for the quick response. I understand.

0 件の賞賛
返信
1,133件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @hxp123 ,

   Your understanding is correct.

  If you do the secure boot, then you also need to prepare the related secure app firmware to match it, and download to the flash, then it will be used correctly.

  If just normal app without the related secure configuration, can't be boot any more, as it lack the sign or secured information.

  More details, please refer to the user manual secure chapter, and our tools: SPT and the MCUbootutlity:

1. SPT

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-s...

 

2. MCUbootutility

https://github.com/JayHeng/NXP-MCUBootUtility/releases/tag/v5.3.0
the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility

 

Wish it helps you!

Best Regards,

Kerry