Does Serial Nor Flash in IMX6 Quad support XIP (eXecute In Place)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does Serial Nor Flash in IMX6 Quad support XIP (eXecute In Place)?

ソリューションへジャンプ
3,054件の閲覧回数
ivyliu
Contributor IV

Hi All,

I am now using IMX6 Quad board with a 4M Serial Nor Flash.

I knew that Parallel Nor Flash can support XIP.

Do you know whether or not Serial Nor Flash in IMX6 Quad can cupport XIP?

Thanks and Best Regards,

Ivy

1 解決策
2,689件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

IMX6 Quad board cannot do that.

QSPI can do that.If you want to do XIP on a serial nor flash please use i.MX6SoloX. 

i.MX6 SoloX M4 Demo image is running on the QSPI.

元の投稿で解決策を見る

4 返答(返信)
2,689件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ivy

xip from i.MX6 ECSPI interface is not supported.

Best regards

igor

2,689件の閲覧回数
ivyliu
Contributor IV

Hi Igor,

Thanks!

Best Regards,

Ivy

0 件の賞賛
返信
2,690件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

IMX6 Quad board cannot do that.

QSPI can do that.If you want to do XIP on a serial nor flash please use i.MX6SoloX. 

i.MX6 SoloX M4 Demo image is running on the QSPI.

2,689件の閲覧回数
ivyliu
Contributor IV

Hi Biyong,

Thanks!

Best Regards,

Ivy

0 件の賞賛
返信