Does Serial Nor Flash in IMX6 Quad support XIP (eXecute In Place)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does Serial Nor Flash in IMX6 Quad support XIP (eXecute In Place)?

跳至解决方案
3,071 次查看
ivyliu
Contributor IV

Hi All,

I am now using IMX6 Quad board with a 4M Serial Nor Flash.

I knew that Parallel Nor Flash can support XIP.

Do you know whether or not Serial Nor Flash in IMX6 Quad can cupport XIP?

Thanks and Best Regards,

Ivy

1 解答
2,706 次查看
BiyongSUN
NXP Employee
NXP Employee

IMX6 Quad board cannot do that.

QSPI can do that.If you want to do XIP on a serial nor flash please use i.MX6SoloX. 

i.MX6 SoloX M4 Demo image is running on the QSPI.

在原帖中查看解决方案

4 回复数
2,706 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ivy

xip from i.MX6 ECSPI interface is not supported.

Best regards

igor

2,706 次查看
ivyliu
Contributor IV

Hi Igor,

Thanks!

Best Regards,

Ivy

0 项奖励
回复
2,707 次查看
BiyongSUN
NXP Employee
NXP Employee

IMX6 Quad board cannot do that.

QSPI can do that.If you want to do XIP on a serial nor flash please use i.MX6SoloX. 

i.MX6 SoloX M4 Demo image is running on the QSPI.

2,706 次查看
ivyliu
Contributor IV

Hi Biyong,

Thanks!

Best Regards,

Ivy

0 项奖励
回复