Does Serial Nor Flash in IMX6 Quad support XIP (eXecute In Place)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does Serial Nor Flash in IMX6 Quad support XIP (eXecute In Place)?

Jump to solution
3,072 Views
ivyliu
Contributor IV

Hi All,

I am now using IMX6 Quad board with a 4M Serial Nor Flash.

I knew that Parallel Nor Flash can support XIP.

Do you know whether or not Serial Nor Flash in IMX6 Quad can cupport XIP?

Thanks and Best Regards,

Ivy

1 Solution
2,707 Views
BiyongSUN
NXP Employee
NXP Employee

IMX6 Quad board cannot do that.

QSPI can do that.If you want to do XIP on a serial nor flash please use i.MX6SoloX. 

i.MX6 SoloX M4 Demo image is running on the QSPI.

View solution in original post

4 Replies
2,707 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ivy

xip from i.MX6 ECSPI interface is not supported.

Best regards

igor

2,707 Views
ivyliu
Contributor IV

Hi Igor,

Thanks!

Best Regards,

Ivy

0 Kudos
Reply
2,708 Views
BiyongSUN
NXP Employee
NXP Employee

IMX6 Quad board cannot do that.

QSPI can do that.If you want to do XIP on a serial nor flash please use i.MX6SoloX. 

i.MX6 SoloX M4 Demo image is running on the QSPI.

2,707 Views
ivyliu
Contributor IV

Hi Biyong,

Thanks!

Best Regards,

Ivy

0 Kudos
Reply