Does Latest Ubuntu Image support Qt5.7?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does Latest Ubuntu Image support Qt5.7?

跳至解决方案
2,229 次查看
xiaochao0131
Contributor III

I installed the ubuntu image for iMX6 sabre lite board, I found the QT5.2.1 has been integrated in it. I need to change QT source code and rebuild it. Does the ubuntu image(i.MX Linux kernel 3.14.52) support the QT5.7 version? 

标签 (3)
0 项奖励
回复
1 解答
2,051 次查看
gary_bisson
Senior Contributor III

Hi,

Qt is not dependent on the kernel version so using the 3.14.52 kernel is not a limitation.

However, Qt5.7 might require some specific versions of some system packages. In other words, if Qt5.7 can be built on Ubuntu Trusty, yes it will work on our image with 3.14.52 kernel.

As a FYI, we are about to release Xenial with kernel 4.1.15 this week.

Regards,

Gary

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,052 次查看
gary_bisson
Senior Contributor III

Hi,

Qt is not dependent on the kernel version so using the 3.14.52 kernel is not a limitation.

However, Qt5.7 might require some specific versions of some system packages. In other words, if Qt5.7 can be built on Ubuntu Trusty, yes it will work on our image with 3.14.52 kernel.

As a FYI, we are about to release Xenial with kernel 4.1.15 this week.

Regards,

Gary

0 项奖励
回复
2,051 次查看
xiaochao0131
Contributor III

Thanks

0 项奖励
回复