Does Latest Ubuntu Image support Qt5.7?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does Latest Ubuntu Image support Qt5.7?

Jump to solution
2,287 Views
xiaochao0131
Contributor III

I installed the ubuntu image for iMX6 sabre lite board, I found the QT5.2.1 has been integrated in it. I need to change QT source code and rebuild it. Does the ubuntu image(i.MX Linux kernel 3.14.52) support the QT5.7 version? 

Labels (3)
0 Kudos
Reply
1 Solution
2,109 Views
gary_bisson
Senior Contributor III

Hi,

Qt is not dependent on the kernel version so using the 3.14.52 kernel is not a limitation.

However, Qt5.7 might require some specific versions of some system packages. In other words, if Qt5.7 can be built on Ubuntu Trusty, yes it will work on our image with 3.14.52 kernel.

As a FYI, we are about to release Xenial with kernel 4.1.15 this week.

Regards,

Gary

View solution in original post

0 Kudos
Reply
2 Replies
2,110 Views
gary_bisson
Senior Contributor III

Hi,

Qt is not dependent on the kernel version so using the 3.14.52 kernel is not a limitation.

However, Qt5.7 might require some specific versions of some system packages. In other words, if Qt5.7 can be built on Ubuntu Trusty, yes it will work on our image with 3.14.52 kernel.

As a FYI, we are about to release Xenial with kernel 4.1.15 this week.

Regards,

Gary

0 Kudos
Reply
2,109 Views
xiaochao0131
Contributor III

Thanks

0 Kudos
Reply