Does IMX8MM MIPI DSI support bus format

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does IMX8MM MIPI DSI support bus format

7,233 次查看
rajvikamdar
Contributor III

 

破坏者
 

Hi Team

 

 

I am getting error on LCD interface over MIPI-DSI, on IMX8MM. We are interfacing ST7796s on the processor and it is giving error of unsupported bus format.

The bus format that the LCD supports is MEDIA_BUS_FMT_RGB666_1X24_CPADHI, which I figured out from the function imx_sec_dsim_encoder_helper_atomic_check() -> bus_format = adjusted_mode->private_flags & 0xffff.

[ 8.557632] ***** RK: 124 imx_sec_dsim_encoder_helper_atomic_check ******
[ 8.557637] $$$$ bus_format: 4117, num_bus_formats = 1 $$$$
[ 8.557637]
[ 8.557639] ***** RK: 128 imx_sec_dsim_encoder_helper_atomic_check ******
[ 8.557642] ****** RK *******
[ 8.557643]
[ 8.557643]
[ 8.557643] RK: pix_clk: 13860
[ 8.557644]
[ 8.557644]
[ 8.557644] RK: bit_clk: 332640
[ 8.557773] ***** RK: 146 imx_sec_dsim_encoder_helper_atomic_check ******
[ 8.557774] ***** RK: 152 imx_sec_dsim_encoder_helper_atomic_check ******
[ 8.557776] ***** RK: 167 imx_sec_dsim_encoder_helper_atomic_check ******
[ 8.557791] imx-lcdif-crtc imx-lcdif-crtc.0: unsupported bus format: 0x1015
[ OK ] Started DNS forwarder and DHCP server.
[ 8.663423] ***** RK: 124 imx_sec_dsim_encoder_helper_atomic_check ******
[ 8.663428] $$$$ bus_format: 4117, num_bus_formats = 1 $$$$
[ 8.663428]
[ 8.663430] ***** RK: 128 imx_sec_dsim_encoder_helper_atomic_check ******
[ 8.663432] ****** RK *******
[ 8.663433]
[ 8.663433]
[ 8.663433] RK: pix_clk: 13860
[ 8.663434]
[ 8.663434]
[ 8.663434] RK: bit_clk: 332640
[ 8.663565] ***** RK: 146 imx_sec_dsim_encoder_helper_atomic_check ******
[ 8.663567] ***** RK: 152 imx_sec_dsim_encoder_helper_atomic_check ******
[ 8.663568] ***** RK: 167 imx_sec_dsim_encoder_helper_atomic_check ******
[ 8.663583] imx-lcdif-crtc imx-lcdif-crtc.0: unsupported bus format: 0x1015
[ OK ] Started Weston Wayland Compositor (on tty7).
[ OK ] Created slice User Slice of UID 0.
Starting User Runtime Directory /run/user/0...
[ OK ] Started User Runtime Directory /run/user/0.
Starting User Manager for UID 0...
[ OK ] Started User Manager for UID 0.
[ OK ] Started Session c1 of user root.
[ 9.388059] ******* RK *******
[ 9.398811]
[ 9.398811] Bus Format return: 0
[ OK ] Started Variscite Bluetooth setup service.
[ OK ] Reached target Multi-User System.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started Update UTMP about System Runlevel Changes.
[ 9.516218] ***** RK: 124 imx_sec_dsim_encoder_helper_atomic_check ******
[ 9.527050] $$$$ bus_format: 4117, num_bus_formats = 1 $$$$
[ 9.527050]
[ 9.540297] ***** RK: 128 imx_sec_dsim_encoder_helper_atomic_check ******
[ 9.550757] ****** RK *******
[ 9.561425]
[ 9.561425]
[ 9.561425] RK: pix_clk: 13860
[ 9.572274]
[ 9.572274]
[ 9.572274] RK: bit_clk: 332640
[ 9.582585] ***** RK: 146 imx_sec_dsim_encoder_helper_atomic_check ******
[ 9.592269] ***** RK: 152 imx_sec_dsim_encoder_helper_atomic_check ******
[ 9.604262] ***** RK: 167 imx_sec_dsim_encoder_helper_atomic_check ******
[ 9.611263] imx-lcdif-crtc imx-lcdif-crtc.0: unsupported bus format: 0x1015

 

How can I check the bus format supported by the processor and LCD module?

0 项奖励
回复
11 回复数

6,751 次查看
bryan_l_courtne
Contributor III

Hi,

Was there a solution to the error message "No hblank data for mode 320x480 with 1 lanes"?

We are getting similar error "No hblank data for mode 240x320 with 1 lanes"

THanks

Bryan

 

0 项奖励
回复

6,986 次查看
rajvikamdar
Contributor III

Hi @joanxie 

 

We are able to resolve the issue, we had to enable the flag MIPI_DSI_CLOCK_NON_CONTINUOUS and use the RGB mode 565 and many more configuration changes. Find attached code directory.

0 项奖励
回复

7,132 次查看
rajvikamdar
Contributor III

Hi @joanxie 

 

Does IMX8MM processor not support the bus format - 0x1015 Why are we getting this error? We need response on this ASAP. Its the issue of processor i think.

When I boot with RGB666, I get the unsupported bus format. But when I boot with RGB666_PACKED, the processor hangs and does not boot up completely. Can you help us please?

 

 

0 项奖励
回复

7,211 次查看
rajvikamdar
Contributor III

Can someone help me on this? Its a bit urgent..

 

 

 

0 项奖励
回复

7,200 次查看
joanxie
NXP TechSupport
NXP TechSupport

what format do you use? rgb666? as I known imx8mm has "imx-lcdif-crtc imx-lcdif-crtc.0: unsupported bus format" message, even you don't connect any displya, what's your output from the lcd? nothing or wrong color?  and what bsp version do you use?

0 项奖励
回复

7,191 次查看
rajvikamdar
Contributor III

Hi @joanxie 

 

Thanks for responding. Yes, our LCD supports RGB666 format. But our LCD is connected over MIPI-DSI interface of the SOM module. So we will have to use the LCDIF CRTC configurations?

We are not getting any display on the LCD screen. We are using BSP: zeus-fsl-5.4.3-mx8mm-v1.1 based on L5.4.3-1.0.0.

Can you please help us urgently on this. We are pretty much stucked.

0 项奖励
回复

7,161 次查看
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the document as below to check if you set the clock correctly

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Setting-i-MX8M-Mini-and-Nano-MIPI-DPHY-C...

0 项奖励
回复

7,157 次查看
rajvikamdar
Contributor III

Yes, we have set the clock according to the attached document. 

Should we get something on the display even if we have error of unsupported bus format?

 

0 项奖励
回复

7,124 次查看
joanxie
NXP TechSupport
NXP TechSupport

did you add your own panel driver? you can refer to the rm6719, which supports MEDIA_BUS_FMT_RGB666_1x18

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/panel/panel-raydium-rm6719...

you also can refer to the topic as below:

https://community.nxp.com/t5/i-MX-Processors/how-to-add-a-new-panel-with-imx8mm-evk-I-got-some-probl...

0 项奖励
回复

7,072 次查看
rajvikamdar
Contributor III

Yes, we have implemented according to the same configurations as attached - rm6719, but we are getting the same error of unsupported bus format.

Please find attached updated code. Could you please help us more? Does IMX8MM not support CPADHI configuration?

0 项奖励
回复

7,022 次查看
rajvikamdar
Contributor III

Hi @joanxie 

 

I resolved the issue of unsupported bus format

we used reference of raydium panel-rm67191 with RGB666_PACKED format settings and modified sitronix panel driver. Find attached driver file. (panel-str-str7796.c)
 
But now we are facing the following issue "No hblank data for mode 320x480 with 1 lanes", the  LCD supports single lane DSI channel. Further  debugging seems that the API: static const struct dsim_hblank_par *sec_mipi_dsim_get_hblank_par () does not have 1 dsi lane support added in the code.
 
We are getting /dev/fb0 as framebuffer, but we are not yet getting any output on the screen.
We are trying to do the following:
 
1. cat /dev/urandom > /dev/fb0
2. gst-launch-1.0 -v videotestsrc ! video/x-raw,width=480,height=320 ! autovideosink
output: FIXME default gstutils.c:3980:gst_pad_create_stream_id_internal:<videotestsrc0:src> Cred
/GstPipeline:pipeline0/GstVideoTestSrc:videotestsrc0.GstPad:src: caps = video/x-raw, format=(string)I420, width=(int)480, height=(int)320, fre
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-raw, format=(string)I420, width=(int)480, height=(int)320, framere
/GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0.GstGhostPad:sink.GstProxyPad:proxypad0: caps = video/x-raw, format=(string)I420, widthe
/GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0/GstWaylandSink:autovideosink0-actual-sink-wayland.GstPad:sink: caps = video/x-raw, fore
/GstPipeline:pipeline0/GstAutoVideoSink:autovideosink0.GstGhostPad:sink: caps = video/x-raw, format=(string)I420, width=(int)480, height=(inte
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-raw, format=(string)I420, width=(int)480, height=(int)320, framee
0:00:00.057853625 528 0x206b00f0 WARN waylandsink wlwindow.c:330:gst_wl_window_new_internal: init surface_state fail, fallb)
 
Have attached Log file - Logs.txt , DTS file: imx8mm-var-dart.dts, driver file: panel-str-str7796.c
 
Can NXP team help us on this.
 
0 项奖励
回复