Does I.MX6Q Have Configurable Generic Processor Bus (Interface) / Enhance Host Controller Interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does I.MX6Q Have Configurable Generic Processor Bus (Interface) / Enhance Host Controller Interface?

1,975 Views
brightwang
Contributor III

As Title My Question Is For That I Need An USB Host Controller Like SAF1760BE With My Selected Application Processor I.MX6Q But Find No Such An Interface In Documents.

SAF1760BEHi-Speed Universal Serial Bus host controller for embedded applications

pastedImage_1.png

But Unfortunately I Can't Find What Is The Interface Between This USB Host Controller And I.MX6Q. The Only Way To Expand The USB Port Seems HSIC USB Host Controller. As You Know There Are Only Few USB Host Controllers With HSIC Interfaces. In Fact Only Microchip Has That Kind Of Parts.

Labels (1)
0 Kudos
Reply
3 Replies

1,868 Views
art
NXP Employee
NXP Employee

The i.MX6Quad processor has the integrated USB Host core with one downstream port with PHY. You can easily expand the number of downstream ports by adding an external USB Hub IC, such as the following ones from Microchip:

http://www.microchip.com/design-centers/usb/usb-hubs-and-devices/products/usb-hubs

or Texas Instruments:

http://www.ti.com/lsds/ti/interface/usb-hub-controller-products.page

or Cypress:

http://www.cypress.com/products/hx2vl

Please note that NXP cannot recommend one vendor/product over another in any way.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,868 Views
brightwang
Contributor III

Hello Artur

Thank You For Your Reply But My Question Is Can It Be Possible To Use SAF1760BE With I.MX6Q?

As You See Here Is An HSIC Bus Bridge With OTG / HOST And Only Microchip Has HSIC Base USB Host Controllers And I Need Them All Are AEC-Q100 Qualified Parts And Won't Use USB Host Port Of I.MX6Q To Expand USB Ports

0 Kudos
Reply

1,868 Views
art
NXP Employee
NXP Employee

Seems that it is possible to use the EIM bus of the i.MX6Q processor to connect the SAF1760BE chip to it. For more details, please refer to the Chapter 22 of the i.MX6Dual/Quad Reference Manual document.

Best Regards,

Artur

0 Kudos
Reply