Does Freescale iMX6 Linux BSP support openAMP?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does Freescale iMX6 Linux BSP support openAMP?

6,891 次查看
mileswang
Contributor II

Hello,

I want to run openAMP on iMX6sx-sdb. ARM A9 core runs Linux and M4 core runs vxWorks.

The communication between A9 and M4 uses openAMP framework.

Does Freescale iMX6 Linux BSP (Yocto project) support openAMP?

Thanks,

Miles

标签 (3)
0 项奖励
回复
5 回复数

5,370 次查看
PetrL
NXP Employee
NXP Employee

Hi,

the support of RPMSG from OpenAMP project is planned for next releases.

Regards,

PetrL

0 项奖励
回复

5,370 次查看
Tarek
Senior Contributor I

Hi Petr,

Can the RPMSG be used for i.MX6Q? I would like to configure it in AMP mode.

3 Cores run Linux and the fourth will run bare-metal.

Is there any example code?

Thanks,

Tarek

0 项奖励
回复

5,366 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Miles

yes it is supported, description can be found in attached Linux Manual

Chapter 53.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

5,366 次查看
mileswang
Contributor II

Hello,

I read the attached Linux Manual Chapter 53 and knew that Freescale’s solution to the multi-core architecture with different OSs is a multi-core communication (MCC) protocol. MCC is different from openAMP.

The key components and capabilities provided by the OpenAMP Framework include remoteproc and RPMsg.

So Freescale Linux doesn't support openAMP. Right?

Best regards,

Miles

0 项奖励
回复

5,366 次查看
igorpadykov
NXP Employee
NXP Employee

right supported only MCC

Best regards

igor

0 项奖励
回复