Does i.MX6UL Processor suport ssi or pcm mode ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6UL Processor suport ssi or pcm mode ?

492 Views
maheshk
Contributor II

Hi all,

I am working on PROGRAMMABLE VOICE DAA SI3050,  It has SPI Interface for control as well as PCM highway data interface, which is to be interfaced with I.MX6UL. Can anybody tell  whether I.MX6UL has SSI interface ?. If this interface is possible, Please share the information on this.

Regards

Mahesh

Labels (1)
0 Kudos
1 Reply

396 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

i.MX6UL has not SSI, instead it has SAI supporting PCM, below part of

i.MX_Linux_Release_Notes.pdf

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos