Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?

ソリューションへジャンプ
2,077件の閲覧回数
harrytan
Contributor I

Hi, I understand that currently i.MX8M BSP is only supported in Linux kernel 4.9.x. Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,920件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Harry

yes there are plans to support i.MX8M in Linux Kernel 4.14.x.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,921件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Harry

yes there are plans to support i.MX8M in Linux Kernel 4.14.x.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,920件の閲覧回数
harrytan
Contributor I

Hi Igor,

Do you know when is estimated release date for the BSP?

Regards,

Harry

0 件の賞賛
返信
1,920件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Harry

seems by the end of year.

Best regards
igor

0 件の賞賛
返信