Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?

跳至解决方案
2,118 次查看
harrytan
Contributor I

Hi, I understand that currently i.MX8M BSP is only supported in Linux kernel 4.9.x. Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
1,961 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Harry

yes there are plans to support i.MX8M in Linux Kernel 4.14.x.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,962 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Harry

yes there are plans to support i.MX8M in Linux Kernel 4.14.x.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,961 次查看
harrytan
Contributor I

Hi Igor,

Do you know when is estimated release date for the BSP?

Regards,

Harry

0 项奖励
回复
1,961 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Harry

seems by the end of year.

Best regards
igor

0 项奖励
回复