Dma interrupts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dma interrupts

3,877件の閲覧回数
garydommer
Contributor I

I have a pcie card mini adapter plugged into a Boundary Devices Nitrogen6 carrier board. the pcie device is a Linear Systems Ttd. SDI Tx card. I got the driver to run however, after some dma buffer transfers the dma done indication as well as the completion interrupt stops. The driver then fills the dma ring and shuts down exiting the test application. At this point the dma will not  restarte unless I reboot the system.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,647件の閲覧回数
wolfgang_muees
Contributor II

in imx-sdma.c, function 

static irqreturn_t sdma_int_handler(int irq, void *dev_id)

replace

if (sdmac->flags & IMX_DMA_SG_LOOP)
sdma_update_channel_loop(sdmac);
else
tasklet_schedule(&sdmac->tasklet);

with

if (sdmac->flags & IMX_DMA_SG_LOOP)
sdma_update_channel_loop(sdmac);
else

mxc_sdma_handle_channel_normal((unsigned long)sdmac);

 

0 件の賞賛
返信

3,647件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Gary

basic pcie validation steps are described in

i.MX6Q PCIe EP/RC Validation System 

please check that for Nitrogen6 correct image configuration is used

GitHub - boundarydevices/linux-imx6: Boundary Devices Kernel tree for i.MX6 

as this is third party board, issue may be posted on meta-fsl-arm mailing list, so that someone

familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,640件の閲覧回数
garydommer
Contributor I

Thankyou Igor. I have submitted subscription request.

All the best,

Gary

0 件の賞賛
返信