About setting pull up/down for GPIO output pin of i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About setting pull up/down for GPIO output pin of i.MX6ULL

3,111 Views
hiectai
Contributor III

Hello everybody.

I'm looking about setting up pull up/down for GPIO output pin for MX6ULL. I'm reading i.MX 6UltraLite Applications Processor Reference Manual. At Output Driver of chapter 26:
• Pull-up, pull-down, and pad keeper are disabled in output mode.
It means that the GPIO in output mode can not set pull-up / down?
Can I set up pull up / down with GPIO in output mode?


Thank you very much!

Labels (2)
2 Replies

2,091 Views
wolfgang_muees
Contributor II

For MX6ULL, Reference Manual Chapter is 29.4.2.2

"Pull-up, pull-down, and pad keeper are disabled in output mode."

I suspect that this statement is FALSE, because in 29.4.2.2.4 "Open Drain", the usage of internal pull up is shown (see Figure 29-8).

So NXP has to clarify.

2,091 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi!

It is possible.

pastedImage_1.png

And you set it in the 32-bit software pad control registers (IOMUXC_SW_PAD_CTL_PAD_<PAD_NAME>

pastedImage_2.png


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos