Display support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Display support

3,539件の閲覧回数
subreh
Contributor I

I'm using the Android Things Starter Kit with the PICO-PI-iMX7 board and the included 5" display.

I'm looking to get a larger display but I'm not entirely sure what the compatibility is. The included display uses an FPC connector (I think?), here's a link to it: https://shop.technexion.com/tdp0500t800480pcap.html

The board lists compatibility for two types of displays:

- 24-bit TTL RGB signals

- MIPI DSI on a 33-pin FPC connector

How would I know if the display is compatible? Do all TTL displays come with the same connector size/compatibility? Or is it like the FPC connector which seems to vary in size? Is there any way to use a standard HDMI monitor?

Thank you

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

3,339件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Subhan,

You can check the datasheet for PicoPi, where you can see the pinout of the conector:

https://www.mouser.mx/pdfdocs/technexion_05242017_PICO-PI-IMX6UL.pdf 

Regards

0 件の賞賛
返信

3,339件の閲覧回数
subreh
Contributor I

Thanks for the reply.

I've checked the datasheet and I think this is the relevant one:

https://www.nxp.com/docs/en/user-guide/PICO-IMX7D-USG.pdf 

I've been looking for displays and I'm not sure how to know if they will be compatible or if I'll need some type of converter. Here are two that I found:

https://www.mouser.co.uk/ProductDetail/Newhaven-Display/NHD-101-1024600AF-ASXV-CTP?qs=sGAEpiMZZMt7dc... 

and

https://www.mouser.co.uk/ProductDetail/Microtips-Technology/MTD0900GZK-1?qs=sGAEpiMZZMu%2FRY1bNe3bO6... 

I'm a beginner to this and am purchasing components for development of my dissertation, and can only buy the components once. Any further help would be much appreciated :smileyhappy:

Thanks

0 件の賞賛
返信

3,339件の閲覧回数
subreh
Contributor I

I've also found the following:

https://www.digikey.co.uk/product-detail/en/olimex-ltd/LCD-OLINUXINO-10TS/1188-1148-ND/5247115

The datasheet for that says it has a 50-pin 24-bit TTL interface, which in my mind is compatible correct?

0 件の賞賛
返信