Display resolution on iMX6 DualLite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Display resolution on iMX6 DualLite

跳至解决方案
1,669 次查看
upendrapatel
Contributor I

I am working on Point of Sale Terminal design with dual display. The maximum display resolution requirement is 1920 x 1080. Can I use iMX6 DualLite processor for this application or will require iMX6 Dual?

0 项奖励
回复
1 解答
1,563 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

In the IMX6SDLRM.pdf you can see that The frame resolution supported is up to 4096x4096 for input and up to 1024x1024 for output. The i.MX6DL has only One IPU, The dual display can work with the maximum display resolution requirement is 1024 x 768. If you want realize dual 1080P display , here recommend you to use i.MX6Q or i.MX6D.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,563 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The i.MX6DualLite processor can not work for this application, so you can consider i.MX6Q and i.MX6Dual.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,564 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

In the IMX6SDLRM.pdf you can see that The frame resolution supported is up to 4096x4096 for input and up to 1024x1024 for output. The i.MX6DL has only One IPU, The dual display can work with the maximum display resolution requirement is 1024 x 768. If you want realize dual 1080P display , here recommend you to use i.MX6Q or i.MX6D.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------