IMX6 solo and DDR3L query

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 solo and DDR3L query

1,568件の閲覧回数
ramesh6663
Contributor III

IMX6 solo MMDC running at up to 396 MHz, Our DDR3L chip is 800MHz.

Queries:

1. How the DDR3L chip frequency down converted to 396MHz and interact with IMX6 solo MMDC controller?

2. Shall we change the frequency of DDR3L through Software? if this is yes please provide me the Details which will help us.

Thanks & Regards,

Rameshkumar

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

1,411件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 It is needed to configure the DDR3 device for 400 MHz.

Please use the following resource how to implement DDR initialization.

DRAM Customization on i.MX6x | NXP Community 

  As for 0S (Linux) level, please refer to Chapter 1 (Porting U-Boot from an i.MX 6/7

Reference Board to an i.MX 6/7 Custom Board) of “i.MX_BSP_Porting_Guide.pdf”
in Linux documentation.

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,411件の閲覧回数
ramesh6663
Contributor III

Can we change DVFS in kernel can we change the DDR frequecy as per product needs?

0 件の賞賛
返信

1,411件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   You may use DVFS, please use NXP Linux documentation about details.

(i.MX_Linux_Reference_Manual.pdf).   

Regards,

Yuri.

0 件の賞賛
返信

1,411件の閲覧回数
ramesh6663
Contributor III

Thanks for your support

0 件の賞賛
返信