Disk encryption using CAAM secure key

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disk encryption using CAAM secure key

ソリューションへジャンプ
7,307件の閲覧回数
jorge_rebollo
Contributor III

Dear all,

I successfully tested meta-imx-fde-demo - imx_sec_apps - i.MX Security Application Examples full disk encryption patch on kernel 4.14 applying patch by hand

I want to integrate it in kernel 4.19 and after applying those patches, also by hand, everything compiles well and key blob is properly generated

However, device mapper launches following error when calling dmsetup

caam_jr 30901000.jr0: caam algorithms can't process tagged key
device-mapper: table: 253:0: crypt: Error decoding and setting key
device-mapper: ioctl: error adding target to table

Development board is MCIMX7SABRE (device status is OPEN)

Linux kernel tested are linux-imx_4.14.78_1.0.0_ga and linux-imx_4.19.35_1.1.0 from linux-imx - i.MX Linux kernel  CodeAurora NXP repository

Reference documentation AN12714 i.MX Encrypted Storage Using CAAM Secure Keys

Can any one give me some help ?

Thanks in advance

Jorge R

ラベル(2)
0 件の賞賛
返信
1 解決策
6,806件の閲覧回数
jorge_rebollo
Contributor III

Hi all,

After been in contact with my local NXP FAE, I would like to share the solution to my problem

This functionality is already available on the L.5.4.47-2.2.0 and the latest L.5.4.70-2.3.0 Linux BSPs

Tested on L.5.4.70-2.3.0 and works as expected !

元の投稿で解決策を見る

6 返答(返信)
5,629件の閲覧回数
haichao
Contributor III

Hi

I follow AN12714 Rev. 0 — 25 February 2020,

I also tested meta-imx-fde-demo - imx_sec_apps - i.MX Security Application Examples full disk encryption patch on kernel 4.14.98 applying patch by hand,but the file in ./mnt/encrypted unencrypted, I do not know why and how to solve.  my platform is imx6ul

thanks

0 件の賞賛
返信
6,807件の閲覧回数
jorge_rebollo
Contributor III

Hi all,

After been in contact with my local NXP FAE, I would like to share the solution to my problem

This functionality is already available on the L.5.4.47-2.2.0 and the latest L.5.4.70-2.3.0 Linux BSPs

Tested on L.5.4.70-2.3.0 and works as expected !

6,960件の閲覧回数
jorge_rebollo
Contributor III

After been in contact with my local NXP FAE, I would like to share the requested functionality is now available in latest Yocto BSP L5.4.47_2.2.0

Not tested yet, but promising it is already official and in NXP BSP mainline !

0 件の賞賛
返信
7,131件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You directly some comments.

Regards,

Yuri.

0 件の賞賛
返信
7,131件の閲覧回数
jorge_rebollo
Contributor III

Hi Yuri,

Thanks for your message

This is my first NXP information request and after revising the information given at NXP technical portal it is not clear to me how to proceed

Do you want me to contact ProSupport ?

Does that require a paid contract between my company and NXP ?

May I have to wait for kernel 5.7 availability and stop trying any other kernel higher than 4.14 ?

I also tested applying demo-caam-blobs 0001-black-key-blob-after-4.14ga-changes-and-license-iden.patch, which is quite similar to kernel 4.14 patch, but with no success on 4.19 disk encryption !

Regards

0 件の賞賛
返信
7,131件の閲覧回数
jorge_rebollo
Contributor III

Yocto Linux BSP used is L4.19.35_1.1.0 downloaded from https://source.codeaurora.org/external/imx/imx-manifest (the latest available when I started working with MCIMX7SABRE last December)

0 件の賞賛
返信