Discussion on RGMII interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Discussion on RGMII interface

3,195 次查看
niteshsahay
Contributor III

Hi

The part MCIMX6QP6AVT1AA has which version of RGMII controller as we need to implement the delay on the PCB accordingly.

BR\Nitesh

标签 (1)
7 回复数

2,911 次查看
niteshsahay
Contributor III

Hi Igor

In my project i am planning to have MAC to MAC communication (RGMII) with MCIMX6QP6AVT1AA.

Any idea on the pins connected for MAC to MAC communication.

Regards

Nitesh

0 项奖励
回复

2,911 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nitesh

RGMII controller is the same as in i.MX6DQ with small differencies described

in EB810 sect.13 Peripherals. PCB routing rules are also the same as for i.MX6DQ,

please check Table 62. RGMII Signal Switching Specifications i.MX6DQP Datasheet

http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6DQPCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,911 次查看
niteshsahay
Contributor III

Hi Igor

Thanks for the reply.

But nowhere it is mentioned as which version of RGMII is supported by IMX6DQ.

BR\Nitesh

0 项奖励
回复

2,911 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nitesh

please look at

Version for RGMII-I/F of i.MX6

~igor

0 项奖励
回复

2,911 次查看
niteshsahay
Contributor III

Hi Igor

The discussion sent does not mentions for which IMX6 it is?

BR\Nitesh

0 项奖励
回复

2,911 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nitesh

it is valid for i.MX6DQ, i.MX6DQP

~igor

2,911 次查看
niteshsahay
Contributor III

Thanks Igor..

Regards

Nitesh

0 项奖励
回复