Hi,
how to remove the login prompt after booting in imx6ulevk using 3.14.38UL BSP package.
I had gone through some of the discussions but didn't get the complete picture. I had to change in inittab. but where can I find the inittab file. When I searched for inittab below are the results. In which file I need to change and then do bitbake.
/home/fsl-release-bsp/core-image-base/tmp/work/cortexa7hf-vfp-neon-poky-linux-gnueabi/busybox/1.23.1-r0/busybox-1.23.1/examples/inittab
/home/fsl-release-bsp/core-image-base/tmp/work/cortexa7hf-vfp-neon-poky-linux-gnueabi/busybox/1.23.1-r0/busybox-1.23.1/examples/bootfloppy/etc/inittab
/home/fsl-release-bsp/core-image-base/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-base/1.0-r0/rootfs/etc/inittab
/home/fsl-release-bsp/core-image-base/tmp/work/imx6ulevk-poky-linux-gnueabi/sysvinit-inittab/2.88dsf-r10/inittab
/home/fsl-release-bsp/core-image-base/tmp/work/imx6ulevk-poky-linux-gnueabi/sysvinit-inittab/2.88dsf-r10/package/etc/inittab
/home/fsl-release-bsp/core-image-base/tmp/work/imx6ulevk-poky-linux-gnueabi/sysvinit-inittab/2.88dsf-r10/packages-split/sysvinit-inittab/etc/inittab
/home/fsl-release-bsp/core-image-base/tmp/work/imx6ulevk-poky-linux-gnueabi/sysvinit-inittab/2.88dsf-r10/image/etc/inittab
/home/fsl-release-bsp/sources/poky/meta/recipes-core/sysvinit/sysvinit-inittab/inittab
Hello Chandra Sekhar,
Please check the following thread for an alternative to do this.
Reg: Auto-Login and run a script Automatically
Regards,