Disable terminal in HDMI of x11 image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable terminal in HDMI of x11 image

1,389 Views
anjojohn
Contributor IV

Hi all,

i have made an core-image-x11 image and tested video display in the HDMI screen. How to remove the terminal that shows in HDMI. I only want my application to be shown on the display. 

0 Kudos
Reply
2 Replies

1,254 Views
b36401
NXP Employee
NXP Employee

You can set "console=none" in u-boot configuration to disable Linux kernel output.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,254 Views
anjojohn
Contributor IV

Hi Victor,

I was talking about the x11 console in the HDMI screen(matchbox-terminal), not the ttymxc UART console.

0 Kudos
Reply