Disable terminal in HDMI of x11 image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disable terminal in HDMI of x11 image

1,388件の閲覧回数
anjojohn
Contributor IV

Hi all,

i have made an core-image-x11 image and tested video display in the HDMI screen. How to remove the terminal that shows in HDMI. I only want my application to be shown on the display. 

ラベル(5)
0 件の賞賛
返信
2 返答(返信)

1,253件の閲覧回数
b36401
NXP Employee
NXP Employee

You can set "console=none" in u-boot configuration to disable Linux kernel output.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,253件の閲覧回数
anjojohn
Contributor IV

Hi Victor,

I was talking about the x11 console in the HDMI screen(matchbox-terminal), not the ttymxc UART console.

0 件の賞賛
返信