Different external memory support between i.MX28 processors?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Different external memory support between i.MX28 processors?

Jump to solution
1,857 Views
lategoodbye
Senior Contributor I

I found differences between the i.MX28 datasheet and Freescale product page according to external RAM support.

From my understanding all i.MX28 processors (including i.MX280) support DDR2. Am i right?

Labels (1)
0 Kudos
Reply
1 Solution
1,686 Views
igorpadykov
NXP Employee
NXP Employee

Hi Stefan

yes right, all i.MX28 processors support DDR2.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,687 Views
igorpadykov
NXP Employee
NXP Employee

Hi Stefan

yes right, all i.MX28 processors support DDR2.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,686 Views
lategoodbye
Senior Contributor I

Thanks

0 Kudos
Reply
1,686 Views
kerryknight
Contributor I

I'm using an i.MX287 with Winbond W972GG6JB-25 2G bit DDR2 SDRAM or W9751G6KB-25 1G bit DDR2 with no problems.  I think the i.MX28 family are fundamentally the same at that level so will all support DDR2 RAM.

0 Kudos
Reply