Different external memory support between i.MX28 processors?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Different external memory support between i.MX28 processors?

ソリューションへジャンプ
2,751件の閲覧回数
lategoodbye
Senior Contributor I

I found differences between the i.MX28 datasheet and Freescale product page according to external RAM support.

From my understanding all i.MX28 processors (including i.MX280) support DDR2. Am i right?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,580件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Stefan

yes right, all i.MX28 processors support DDR2.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,581件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Stefan

yes right, all i.MX28 processors support DDR2.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,580件の閲覧回数
lategoodbye
Senior Contributor I

Thanks

0 件の賞賛
返信
2,580件の閲覧回数
kerryknight
Contributor I

I'm using an i.MX287 with Winbond W972GG6JB-25 2G bit DDR2 SDRAM or W9751G6KB-25 1G bit DDR2 with no problems.  I think the i.MX28 family are fundamentally the same at that level so will all support DDR2 RAM.

0 件の賞賛
返信