Different OrCAD format needed for SABRE-SD schematic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Different OrCAD format needed for SABRE-SD schematic

Jump to solution
1,942 Views
ScottKerstein
Contributor III

Hello,

 

Referring to the i.MX6 SABRE-SDB and –SDP reference designs, Freescale is providing these files in OrCAD Capture version 16.3 or later.  This is not compatible with earlier versions of OrCAD or any of the conversion utilities provided by Altium.

 

I'm looking for a version to support Altium versions 9, 10 and 13, and/or OrCAD version 16.0.

 

DSN files are attached if someone within the community wanted to convert, that would be appreciated.

 

Thanks in advance.

Scott

Original Attachment has been moved to: SPF-27516_C4.zip

Labels (1)
0 Kudos
Reply
1 Solution
1,714 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
1,715 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,714 Views
Yuri
NXP Employee
NXP Employee

  Please try the enclosed file in OrCad 16.2 format.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply