How to read a CPUNUM_CORES value for i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to read a CPUNUM_CORES value for i.MX6

ソリューションへジャンプ
1,289件の閲覧回数
yuuki
Senior Contributor II

Dear All,

We'd like to read the value of CPUNUM_CORES:0x430 [21:20] to check the CPU type.

We understand that this value is read by using OCOTP_CTRL.

However, We do'nt understand this step.

Would you teach how to read a CPUNUM_CORES value by using OCOTP_CTRL?

Best Regards,

Yuuki

ラベル(1)
0 件の賞賛
返信
1 解決策
1,198件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,199件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
1,198件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

for OCOTP_CTRL usage please look at SDK example ..ocotp/src/ocotp.c

i.MX 6Series Platform SDK : Bare-metal SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信